3.3V regulator with lithium ion coin cell battery

I need the supply voltage to be stable at the same value while the application is running. This is because I’m comparing analog input voltages (that are based off of the supply voltage) to threshold voltage values in the microcontroller, so I don’t want the input voltages to change if the battery voltage fluctuates.