# 315/433 Mhz data links pt.1 @1200 bps

**URL:** <https://community.sparkfun.com/t/315-433-mhz-data-links-pt-1-1200-bps/22168>\
**Category:** Wireless & IoT\
**Created:** [October 6, 2011, 7:44pm UTC](https://community.sparkfun.com/t/315-433-mhz-data-links-pt-1-1200-bps/22168 "2011-10-06T19:44:06Z")\
**Posts on this page:** 1\
**Page:** 1

<div class="post-metadata">

**Author:** ![another-dave](https://avatars.discourse-cdn.com/v4/letter/a/c4cdca/32.png) [@another-dave](https://community.sparkfun.com/u/another-dave)\
**Post date:** [October 6, 2011, 7:44pm UTC](https://community.sparkfun.com/t/315-433-mhz-data-links-pt-1-1200-bps/22168/1 "2011-10-06T19:44:06Z")

</div>

I’ve been trying to re-create some stuff I did with these as there appears to be the idea that they are cr@p. Unfortunately I no longer am employed where I did the work and my “backup” was on a laptop that whas stolen years ago.

But I hooked a PIC12F675 (with a little bit of test code to the 315MHz xmtr and took some ‘scope pics of what I was sending in on the data line of the xmtr and what I was getting out of the 4800 bps recvr boards’ data pin. I didn’t use the latest incarnation of these sparkfun boards so your mileage may vary.

you can see that:

1.) the AGC needs to be “trained” and that the initial data is gibberish. After 4 bytes it’s good.

2.) there is a limit to the leading /training edges that limits the bps usefulness for p/w modulation encoding decoding (have to go down to about 1200 bps to get good edge resolution making p/w modulation feasible).

3.) the AGC breaks look after a period of non use, the higher the bit rate the quicker it breaks lock.

the code for this was VERY simple:

'oshon basic for PICs on a PIC1F675

'how many pulse bursts @ ~1200bps does it take to optimise the agc of the $5 revr?

'use a 25% d/c

'each Bit consists of 4 time slices of ~ 208usec

'for each 8 bit character there is a 4 bit(16 time slice)intercharacter logic low

'pin1 vcc

'pin2 GP5 output serial stream

'pin8 return

TRISIO = %001000

GPIO = 0

Dim x As Byte

Dim y As Byte

Dim burst As Byte

Dim burst\_count As Byte

main:

'init variables

WaitMs 5000

burst\_count = 4

For burst = 1 To burst\_count

For x = 1 To 8

GPIO.5 = 1

WaitUs 208

Toggle GPIO.5

WaitUs 624

Next x

For y = 1 To 4

GPIO.5 = 0

WaitUs 832

Next y

Next burst

End

here’s some pics @1200 bps I’ll upload some @4800 in a second message for comparison.

-Ignore time bases in photos except ones with cursors, time base doesn’t work in “zoom function” I used to zoom in on areas of trace memory.

-the bottom trace is the input into the transmitter, the top is the output from the receiver.

-the file names give a description of the picture