# Analog input to halt timer problem

**URL:** <https://community.sparkfun.com/t/analog-input-to-halt-timer-problem/26854>\
**Category:** Arduino\
**Created:** [June 3, 2013, 12:17pm UTC](https://community.sparkfun.com/t/analog-input-to-halt-timer-problem/26854 "2013-06-03T12:17:52Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![c2crider](https://avatars.discourse-cdn.com/v4/letter/c/ecb155/32.png) [@c2crider](https://community.sparkfun.com/u/c2crider)\
**Post date:** [June 3, 2013, 12:17pm UTC](https://community.sparkfun.com/t/analog-input-to-halt-timer-problem/26854/1 "2013-06-03T12:17:52Z")

</div>

Hi there,

I am using arduino for a project, and despite progressing fairly well to start with, I’ve hit a bit of a brick wall with a problem.

Essentially, I want to stop a timer when the value on an analogue input reaches a certain point. I am using a Sharp IR sensor as my analogue input.

I’ve tried various “if” and “else if” commands with limited success, would anyone be able to help me out?

```auto
 #define ledPin 13 // LED connected to digital pin 13
#define buttonPin 7 // button on pin 7
#define analoguePin A0

int value = LOW; // previous value of the LED
int buttonState; // variable to store button state
int lastButtonState; // variable to store last button state
int blinking; // condition for blinking - timer is timing
long interval = 100; // blink interval - change to suit
long previousMillis = 0; // variable to store last time LED was updated
long startTime ; // start time for stop watch
long elapsedTime ; // elapsed time for stop watch
int fractional; // variable used to store fractional part of time
int analogueIn = A0;
int sensorValue = 0; // value read from the pot
int outputValue = 0; // value output to the PWM (analog out)
int analogueState;

void setup()
{
   Serial.begin(9600);

   pinMode(ledPin, OUTPUT); // sets the digital pin as output

   pinMode(buttonPin, INPUT); // not really necessary, pins default to INPUT anyway
   pinMode(analoguePin, INPUT);
   digitalWrite(buttonPin, HIGH); // turn on pullup resistors. Wire button so that press shorts pin to ground.
   
}

void loop()
{
    // check for button press
   buttonState = digitalRead(buttonPin); // read the button state and store
   
   sensorValue = analogRead (analogueIn);
  
 if (sensorValue = 300) analogueState = LOW; 
  else if (sensorValue = 500)analogueState = HIGH;
 
  
   if (buttonState == LOW && lastButtonState == HIGH && blinking == false){ // check for a high to low transition
      // if true then found a new button press while clock is not running - start the clock

      startTime = millis(); // store the start time
      blinking = true; // turn on blinking while timing
      delay(5); // short delay to debounce switch
      lastButtonState = buttonState; // store buttonState in lastButtonState, to compare next time

   }

   else if (analogueState == LOW && lastButtonState == HIGH && blinking == true){ // check for a high to low transition
      // if true then found a new button press while clock is running - stop the clock and report

        elapsedTime = millis() - startTime; // store elapsed time
        blinking = false; // turn off blinking, all done timing
        lastButtonState = buttonState; // store buttonState in lastButtonState, to compare next time

       // routine to report elapsed time 
        Serial.print( (int)(elapsedTime / 1000L)); // divide by 1000 to convert to seconds - then cast to an int to print

        Serial.print("."); // print decimal point

        // use modulo operator to get fractional part of time 
       fractional = (int)(elapsedTime % 1000L);

       // pad in leading zeros - wouldn't it be nice if 
       // Arduino language had a flag for this? :)
       if (fractional == 0)
          Serial.print("000"); // add three zero's
       else if (fractional < 10) // if fractional < 10 the 0 is ignored giving a wrong time, so add the zeros
          Serial.print("00"); // add two zeros
       else if (fractional < 100)
          Serial.print("0"); // add one zero

       Serial.println(fractional); // print fractional part of time 

   }

   else{
      lastButtonState = buttonState; // store buttonState in lastButtonState, to compare next time
   }

   // blink routine - blink the LED while timing
   // check to see if it's time to blink the LED; that is, the difference
   // between the current time and last time we blinked the LED is larger than
   // the interval at which we want to blink the LED.

   if ( (millis() - previousMillis > interval) ) {

      if (blinking == true){
         previousMillis = millis(); // remember the last time we blinked the LED

         // if the LED is off turn it on and vice-versa.
         if (value == LOW)
            value = HIGH;
         else
            value = LOW;
         digitalWrite(ledPin, value);
      }
      else{
         digitalWrite(ledPin, LOW); // turn off LED when not blinking
      }
   }

}

```

I’m sure to a more experienced user this is child’s play! Thank you for your time in advance

Andrew

---

<div class="post-metadata">

**Author:** ![Mee\_n\_Mac](https://avatars.discourse-cdn.com/v4/letter/m/aeb1de/32.png) [@Mee\_n\_Mac](https://community.sparkfun.com/u/Mee_n_Mac)\
**Post date:** [June 7, 2013, 10:28pm UTC](https://community.sparkfun.com/t/analog-input-to-halt-timer-problem/26854/2 "2013-06-07T22:28:23Z")

</div>

I haven’t had a chance to figure out all the things you want your code to do (there seem to be a lot of conditionals) but I did notice the following;

```auto
 if (sensorValue = 300) analogueState = LOW;
  else if (sensorValue = 500)analogueState = HIGH;

```

If see 3 things wrong with the above. First the _test for equality_ is ==, not =.

[http://arduino.cc/en/Reference/If](http://arduino.cc/en/Reference/If)

Second is you’re looking for exact values, 300 and 500. You may be unlucky and get 299 or 501 w/o the arduino ever seeing 300 or 500. Do you want a window (ie : 300+/- 10) or perhaps just a threshold (ie : \<= 300 or \>= 500) ?

Are you looking to stop the timer upon the 2’nd button push or when the analog value gets above (? or below ?) some value (500) ? How did you want the timer to start ? Upon 1’st button push ? Or button push and analog value \< 300 ?