I notice now that Telit have updated their product line. The GC864 models are much smaller than the GM862 but have the same benefit of a connector which the GE863 does not have.
Also they now have the UC864 which is Quadband GSM and Triband UTMS/HSDPA drooool :shock:
Sorry to resurrect a dead thread, but… If sparkfun is not planning on producing this item, would it be possible to publish the schematic so that the rest of us might benefit from the work that you did do?
I would have much interest in a ge863 board. Especially if Sparkfun mounted the GE863-PRO³ on it. This paticular variant can run LINUX. Just consider the possibilities of a tiny module with full linux that speaks IP over GSM. Note, when I spoke with the telit rep I was advised not to use the 862 module due to it’s being end of life. It’s time to update the board and offer the 863 running linux and/or the 864 series where you can use one board and module family for gsm, umts, or cdma - just choose the module in that family for the technology you need. 2 boards would be the best option one with connector for the 864 family and the other with an 863pro3-linux mounted.