# Basic ADXL345 issues

**URL:** <https://community.sparkfun.com/t/basic-adxl345-issues/24777>\
**Category:** Arduino\
**Created:** [August 10, 2012, 12:24am UTC](https://community.sparkfun.com/t/basic-adxl345-issues/24777 "2012-08-10T00:24:26Z")\
**Posts on this page:** 1\
**Page:** 1

<div class="post-metadata">

**Author:** ![MasterPlanDan42](https://avatars.discourse-cdn.com/v4/letter/m/46a35a/32.png) [@MasterPlanDan42](https://community.sparkfun.com/u/MasterPlanDan42)\
**Post date:** [August 10, 2012, 12:24am UTC](https://community.sparkfun.com/t/basic-adxl345-issues/24777/1 "2012-08-10T00:24:26Z")

</div>

To anyone who feels like helping out a newbie:

I recently purchased an Arduino Uno and ADXL345 breakout board with the intention of doing some tilt-sensing applications. I downloaded the sample SPI code available from Sparkfun’s quickstart guide ([http://www.sparkfun.com/tutorials/240](http://www.sparkfun.com/tutorials/240)):

```auto
//Add the SPI library so we can communicate with the ADXL345 sensor
#include <SPI.h>

//Assign the Chip Select signal to pin 10.
int CS=10;

//This is a list of some of the registers available on the ADXL345.
//To learn more about these and the rest of the registers on the ADXL345, read the datasheet!
char POWER_CTL = 0x2D;	//Power Control Register
char DATA_FORMAT = 0x31;
char DATAX0 = 0x32;	//X-Axis Data 0
char DATAX1 = 0x33;	//X-Axis Data 1
char DATAY0 = 0x34;	//Y-Axis Data 0
char DATAY1 = 0x35;	//Y-Axis Data 1
char DATAZ0 = 0x36;	//Z-Axis Data 0
char DATAZ1 = 0x37;	//Z-Axis Data 1

//This buffer will hold values read from the ADXL345 registers.
char values[10];
//These variables will be used to hold the x,y and z axis accelerometer values.
int x,y,z;

void setup(){ 
  //Initiate an SPI communication instance.
  SPI.begin();
  //Configure the SPI connection for the ADXL345.
  SPI.setDataMode(SPI_MODE3);
  //Create a serial connection to display the data on the terminal.
  Serial.begin(9600);
  
  //Set up the Chip Select pin to be an output from the Arduino.
  pinMode(CS, OUTPUT);
  //Before communication starts, the Chip Select pin needs to be set high.
  digitalWrite(CS, HIGH);
  
  //Put the ADXL345 into +/- 4G range by writing the value 0x01 to the DATA_FORMAT register.
  writeRegister(DATA_FORMAT, 0x01);
  //Put the ADXL345 into Measurement Mode by writing 0x08 to the POWER_CTL register.
  writeRegister(POWER_CTL, 0x08); //Measurement mode  
}

void loop(){
  //Reading 6 bytes of data starting at register DATAX0 will retrieve the x,y and z acceleration values from the ADXL345.
  //The results of the read operation will get stored to the values[] buffer.
  readRegister(DATAX0, 6, values);

  //The ADXL345 gives 10-bit acceleration values, but they are stored as bytes (8-bits). To get the full value, two bytes must be combined for each axis.
  //The X value is stored in values[0] and values[1].
  x = ((int)values[1]<<8)|(int)values[0];
  //The Y value is stored in values[2] and values[3].
  y = ((int)values[3]<<8)|(int)values[2];
  //The Z value is stored in values[4] and values[5].
  z = ((int)values[5]<<8)|(int)values[4];
  
  //Print the results to the terminal.
  Serial.print(x, DEC);
  Serial.print(',');
  Serial.print(y, DEC);
  Serial.print(',');
  Serial.println(z, DEC);      
  delay(10); 
}

//This function will write a value to a register on the ADXL345.
//Parameters:
// char registerAddress - The register to write a value to
// char value - The value to be written to the specified register.
void writeRegister(char registerAddress, char value){
  //Set Chip Select pin low to signal the beginning of an SPI packet.
  digitalWrite(CS, LOW);
  //Transfer the register address over SPI.
  SPI.transfer(registerAddress);
  //Transfer the desired register value over SPI.
  SPI.transfer(value);
  //Set the Chip Select pin high to signal the end of an SPI packet.
  digitalWrite(CS, HIGH);
}

//This function will read a certain number of registers starting from a specified address and store their values in a buffer.
//Parameters:
// char registerAddress - The register addresse to start the read sequence from.
// int numBytes - The number of registers that should be read.
// char * values - A pointer to a buffer where the results of the operation should be stored.
void readRegister(char registerAddress, int numBytes, char * values){
  //Since we're performing a read operation, the most significant bit of the register address should be set.
  char address = 0x80 | registerAddress;
  //If we're doing a multi-byte read, bit 6 needs to be set as well.
  if(numBytes > 1)address = address | 0x40;
  
  //Set the Chip select pin low to start an SPI packet.
  digitalWrite(CS, LOW);
  //Transfer the starting register address that needs to be read.
  SPI.transfer(address);
  //Continue to read registers until we've read the number specified, storing the results to the input buffer.
  for(int i=0; i<numBytes; i++){
    values[i] = SPI.transfer(0x00);
  }
  //Set the Chips Select pin high to end the SPI packet.
  digitalWrite(CS, HIGH);
}

```

I then hooked everything up as indicated in the guide, and got good results. Satisfied, I breadboarded the project, and happy with that, transferred everything off of a breadboard to protoboard and soldered everything up. It was at this point that things went bad.

After getting unexpected behavior, I detached the ADXL345 from the rest of the project and hooked it up to the Arduino as I had before. The only output from any of the axes appearing on the serial monitor was a steady “-1”. Figuring that I had busted the accelerometer in the process of soldering wires (either heat damage or an accidental short seemed possible), I grit my teeth and ordered a new breakout from Sparkfun.

When the new one came in, I carefully set it up as before, only to get the same error. Figuring that something might be wrong with the Arduino at this point, I checked the 3.3V power supply with my multimeter and found that while it would output a steady 3.3V with nothing attached to it, as soon as I attached it to the ADXL345 it shot up to around 4.5V.

At this point, I’m not sure whether the Arduino is busted, whether (through extraordinary bad luck) the ADXL345 is busted, or both. I’m aware that I didn’t use a level converter to bring the Arduino data lines down to 3.3V, but the quickstart guide indicated that this might not be necessary for short-term applications. It might be worth mentioning that while the old ADXL345 was operated (successfully, if temporarily) in parallel with a few other devices on a SPI bus, the new one was only ever directly connected to the Arduino.

This is my first post to the forum. I was hoping that anyone with experience on these kind of issues might be able to help me figure out which component is busted, or at least give me some idea of what to check. Thanks for enduring the long post, and thanks in advance to anyone who helps me out!