sspbass:
I like it but the order seems a bit odd.Shouldn’t the Save menu be last in the sequence?
Also, shouldn’t the number of hits and the time out menus be after the CoF is selected as well as only displaying the one that is needed.
i.e. if I’m setting the number of hits I want to time to there’s no need to select the time out time, it should just be set to the max.
When you get into that series of menus, you first land on the Select CoF : menu. From there you can go either right or left after choosing (or not !) a CoF.
Left would get you to the Save Options : menu, which will allow you to exit after choosing the CoF. Exit and use would be the first choice, presumably the most used after selecting a CoF and not modifying anything about it.
Right will get you to the Select # of shooters :, which I thought might be the most usually changed preset from a presaved CoF.
Going right from there will get you to the countdown delay menu.
Going right again will then get you to the stop hits menu.
Going right yet again will then get you to the stop time menu.
Going right once more will then get you to the Save Options : menu, where you can elect to save all the presets you’ve just changed. So it’s last after going through all the things you might want to change.
But since it’s all a big ring, you can opt to go left, left, left to get to the menu item you want to change the preset you want to change. Or left, left, right …
Of course the order of the displays/menus can be changed, it all depends on which items you think will be most used and therefore should be closer to the “home” menu you land on when you first get into this UI. My thinking was you’d have timed CoFs or hit limited CoFs already setup, so choosing one of those from a list would be the most common. Thereafter it would be either :
-
altering the # of shooters, as a friend may want to join in the fray or
-
just exitting the menus to use the CoF selected.
So these were placed 1 button push away from the “home” menu. The order of the others was my best guess at some late AM hour. :mrgreen: