Alright I will try it and report back here in a few days.
(Long Story short: swapping the ESP32 for the Teensy did not solve the LED strip timeout issues possibly related to clock stretching, but made it worse)
OK it took me some time to get the Teensy working, but now I can share results:
Quick summarize: I ran into the problem that as soon as I added the Qwiic LED strip to the system, it became unstable. Sometimes the LEDs did not update correctly, and after a few minutes of usage āhardware I2C ackā errors startet to popup in the console. Changing clock speeds or other solutions suggested here did not help (better soldering, shorter cables etc.)
@paulvha suggested to use a Teensy processor instead of the ESP32 as the Teensy supports clock strechting which the ESP32 does not. It was suggested that the LED strip uses clock stretching and therefore the hardware timeouts occur.
So now I have swapped the ESP32 to the Teensy - but unfortunately, the problem persists. The same issues happen, the only difference is that this time I do not get random āhardware I2C ackā errors that get more over time until the board crashes - with the Teensy, the board crashes immediately after a few minutes of usage. If it crashes, there is nothing that continues to work on the Qwiic bus. Only a power cycle allows restart (the RST button on the Micromod Board does not do anything on the Teensy, but thats probably another story).
Anyways. If I remove the LED strip, everything so far works fine.
So maybe I am just doomed to not use LED lighting in the project if I stay with the Qwiic / Sparkfun ecosystem⦠![]()
(As for the suggestion to use Softwire, I still have to look into this but at the moment I need to go forward, so leave the LED strip aside..)
Have you tried one of the examples of the LED ? If that works add other devices. Maybe there is another conflict.
Yes I have, and I am pretty sure the conflict starts as soon as I add both the BNO086 IMU and the LED strip together. When I leave one of them out, the other one runs smooth.
I havenāt tested that with the Teensy but with the ESP32 it was like that.
If I find time today, Iād like to try and see what happens if I do not use all 10 but just 1 LED, maybe that easens the load on the I2C bus enough so it will work.
The IMU is a must-have. If I wonāt get LED strip to work, as alternative I thought about adding a second Qwiic button that is not interactable by the user but it also has a nice single LED that can be controlled; the Qwiic button LED worked flawless so far.
Using only 1 LED instead of all 10 did not help either.
The entire setup crashes after a few minutes into play, starting with the usual error behaviour (a few wrong color flashes or colors, then crash).
For everyone else coming here, I have followed a suggestion by a SparkFun employee in another thread āAlternative for Qwiic LED Strip?ā and it solved the issue.
Solution: use Muxer to isolate IMU from LED Strip and therefore prevent issues with clock stretching on some CPUs.
Dang, i didnāt know that worked to combat clock stretching. Thanks for sharing!
Iād like to share another finding I made as the stability seems to be directly linked to the power demand/supply:
- with ESP32 (instead of Teensy) I still got the occasional wrong colors, followed by I2C crashes
- Iāve then cut the 3.3V power supply as mentioned in the hookup guide and connected the LED strip to an external power source via VIN (power comes from PoE Micromod Board).
- With that external power supply, all stability issues are gone. The strip works perfect, even with rapid changes in color and brightness.
So maybe the muxer and/or clock stretching isnāt necessary / the reason after all. But I keep it for a completely separate reason.
(Link to post: Alternative for Qwiic LED Strip? - #8 by michaelheiml82)