# EEPROM Error - MLX90640 (SEN-14843)

**URL:** <https://community.sparkfun.com/t/eeprom-error-mlx90640-sen-14843/36912>\
**Category:** Imaging\
**Created:** [May 20, 2019, 8:29pm UTC](https://community.sparkfun.com/t/eeprom-error-mlx90640-sen-14843/36912 "2019-05-20T20:29:17Z")\
**Posts on this page:** 3\
**Page:** 1

<div class="post-metadata">

**Author:** ![S\_Jafri](https://avatars.discourse-cdn.com/v4/letter/s/58f4c7/32.png) [@S\_Jafri](https://community.sparkfun.com/u/S_Jafri)\
**Post date:** [May 20, 2019, 8:29pm UTC](https://community.sparkfun.com/t/eeprom-error-mlx90640-sen-14843/36912/1 "2019-05-20T20:29:17Z")

</div>

Hi,

We recently received two of the[[IR Array Breakout Boards (V12)](https://www.sparkfun.com/products/14843) but we have run into the same error regarding EEPROM Parameter. Currently we are using these boards with the [[Melexis Evaluation board](https://www.melexis.com/en/product/EVB90640-41/Evaluation-Board-MLX90640) and using their software to get the imaging. We do have a breakout board (V10) we purchased previously that works with the Evaluation board with no issues. I’ve attached screenshots of the error as well as a picture of our setup (Note: we are currently using the QWICC connection for this setup, the soldered wires just lead out to an unplugged connector that would be used to connect to the Melexis Evaluation board). Is there anything we can do to resolve these EEPROM errors we are getting on the new boards?]([Error - Melexis](https://www.melexis.com/en/product/EVB90640-41/Evaluation-Board-MLX90640))]([SparkFun IR Array Breakout - 110 Degree FOV, MLX90640 (Qwiic) - SEN-14843 - SparkFun Electronics](https://www.sparkfun.com/products/14843))

 ![Melexis Evaluation Board w IR Array.jpg](https://canada1.discourse-cdn.com/sparkfun/original/3X/a/0/a00164aa00059ae0bbedbfbf7b44f01c2e2ba868.jpeg)

![Thermal Camera Error 2.JPG](https://canada1.discourse-cdn.com/sparkfun/original/3X/8/c/8c91a8eb00b9a2fd34487b59f8a85f44a527bd07.jpeg)

![Thermal Camera Error 1.JPG](https://canada1.discourse-cdn.com/sparkfun/original/3X/3/7/37aaf810a8e4e5034175f10ab14a2b4f403c9d1a.jpeg)

---

<div class="post-metadata">

**Author:** ![El\_Duderino](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/el_duderino/32/6367_2.png) [@El\_Duderino](https://community.sparkfun.com/u/El_Duderino)\
**Post date:** [May 23, 2019, 3:35pm UTC](https://community.sparkfun.com/t/eeprom-error-mlx90640-sen-14843/36912/2 "2019-05-23T15:35:40Z")

</div>

Hi S\_Jafri,

Unfortunately, we cannot help you out too much with this issue since we do not carry the Melexis Evaluation Board so it is impossible for us to try and recreate your issue. Since it is working with the previous revision of the board, the issue is most likely with the MLX90640 breakouts but without testing on in an Arduino environment like our [[Hookup Guide](https://learn.sparkfun.com/tutorials/qwiic-ir-array-mlx90640-hookup-guide) covers, I am not sure what the issue might be. If possible, try testing the sensors with our Arduino library or at least run an I2C scan to see if the bus can detect the MLX90640.

We found with other users that testing the SDA and SCL lines for resistance/continuity to ground helps identify a defect. If you have a multimeter, try measuring resistance and testing for continuity with GND while the sensor is unpowered.]([Qwiic IR Array (MLX90640) Hookup Guide - SparkFun Learn](https://learn.sparkfun.com/tutorials/qwiic-ir-array-mlx90640-hookup-guide))

---

<div class="post-metadata">

**Author:** ![S\_Jafri](https://avatars.discourse-cdn.com/v4/letter/s/58f4c7/32.png) [@S\_Jafri](https://community.sparkfun.com/u/S_Jafri)\
**Post date:** [June 10, 2019, 9:33pm UTC](https://community.sparkfun.com/t/eeprom-error-mlx90640-sen-14843/36912/3 "2019-06-10T21:33:17Z")

</div>

Hi TS-Mark,

So we’ve tried setting up the MLx90640 breakout boards using the Arduino hookup guide you linked and a Teensy 3.5 as the microcontroller. We had no issue using the V10 board but when we used the V12 boards the following is shown:

"MLX90640 IR Array Example

MLX90640 online!

Parameter extraction failed

Pixel 0: nanC

Pixel 1: nanC

Pixel 2: nanC

Pixel 3: nanC

Pixel 4: nanC

Pixel 5: nanC

Pixel 6: nanC

Pixel 7: nanC

Pixel 8: nanC

Pixel 9: nanC"

We also used the I2C Scanner you mentioned on got the following message:

"I2C Scanner

Scanning…

I2C device found at address 0x33 !

done"

We did find that if we start the programs with the V10 board and swap to one of the V12 boards we were able to get readings, however this wouldn’t be ideal for our application. Do you have any suggestions on how we can further troubleshoot these boards?