# ESP8266 http request

**URL:** <https://community.sparkfun.com/t/esp8266-http-request/37180>\
**Category:** Wifi\
**Created:** [June 28, 2019, 8:21pm UTC](https://community.sparkfun.com/t/esp8266-http-request/37180 "2019-06-28T20:21:53Z")\
**Posts on this page:** 6\
**Page:** 1

<div class="post-metadata">

**Author:** ![dakota99](https://avatars.discourse-cdn.com/v4/letter/d/76d3ee/32.png) [@dakota99](https://community.sparkfun.com/u/dakota99)\
**Post date:** [June 28, 2019, 8:21pm UTC](https://community.sparkfun.com/t/esp8266-http-request/37180/1 "2019-06-28T20:21:53Z")

</div>

Hello

I 'm using Sparkfun ESP8266. I have followed this tutorial :

[https://learn.sparkfun.com/tutorials/ … 6351479]

I have run the ESP8266\_SHIELD\_DEMO project. The device is responding properly.

The server mode is working. The board has an ip adress.

When I go to his Ip adress I get the values of analogic ports. Everything works fine.

I would like to send an http request to the board with a parameter for example : [http://192.168.0.38/?param1=P1](http://192.168.0.38/?param1=P1)

This parameter must be retrieved in the Arduino and fire an action.

My question :

What is the code for receiving the httprequest ?

What is the syntax of httprequest ? I have tried

Here below this is the code I have tested without success.

Thanks for your help.

Mario

```auto
void serverDemo()
{
  ESP8266Client client = server.available(500);
  
  if (client) 
  {
    Serial.println(F("Client Connected!"));
    boolean currentLineIsBlank = true;// an http request ends with a blank line
    while (client.connected()) 
    { if (client.available()) 
      {
        char c = client.read();
        header += c;
        if (c == '\n' && currentLineIsBlank) 
        { Serial.println(header);
          if (header.indexOf("P1") >= 0) {
          Serial.println("IT WORKS");}
          
          Serial.println(F("Sending HTML page"));
          String htmlBody;
          client.print("test");
          break;
        }
        if (c == '\n') 
        {
          currentLineIsBlank = true; // you're starting a new line

        }
        else if (c != '\r') 
        {
          currentLineIsBlank = false; // you've gotten a character on the current line
        }
      }
    }
    delay(1); // give the web browser time to receive the data
    client.stop(); // close the connection:
    Serial.println(F("Client disconnected"));
  }
}

```

---

<div class="post-metadata">

**Author:** ![dakota99](https://avatars.discourse-cdn.com/v4/letter/d/76d3ee/32.png) [@dakota99](https://community.sparkfun.com/u/dakota99)\
**Post date:** [July 6, 2019, 5:57am UTC](https://community.sparkfun.com/t/esp8266-http-request/37180/2 "2019-07-06T05:57:35Z")

</div>

Hello,

This is the entire code

The readString variable which should contain the parameter, is empty.

Thanks for your help.

```auto
#include <SoftwareSerial.h> 
#include <SparkFunESP8266WiFi.h>
const char mySSID[] = "";
const char myPSK[] = "";
String readString; //create readString class
String cm1; 
String cm2; 
ESP8266Server server = ESP8266Server(80);

void setup() 
{
  Serial.begin(9600);
  initializeESP8266();
  connectESP8266();
  displayConnectInfo();
  serverSetup();
}

void loop() 
{
  serverDemo();
}

void initializeESP8266()
{
  int test = esp8266.begin();
  if (test != true)
  {
    Serial.println(F("Error talking to ESP8266."));
    errorLoop(test);
  }
  Serial.println(F("ESP8266 Shield Present"));
}

void connectESP8266()
{
  // The ESP8266 can be set to one of three modes:
  // 1 - ESP8266_MODE_STA - Station only
  // 2 - ESP8266_MODE_AP - Access point only
  // 3 - ESP8266_MODE_STAAP - Station/AP combo
  // Use esp8266.getMode() to check which mode it's in:
  int retVal = esp8266.getMode();
  if (retVal != ESP8266_MODE_STA)
  { // If it's not in station mode.
    // Use esp8266.setMode([mode]) to set it to a specified mode.
    // retVal = esp8266.setMode(ESP8266_MODE_STA);
    retVal = esp8266.setMode(ESP8266_MODE_AP);
    if (retVal < 0)
    {
      Serial.println(F("Error setting mode."));
      errorLoop(retVal);
    }
  }
  Serial.println(F("Mode set to station"));
  retVal = esp8266.status();
  if (retVal <= 0)
  {
    Serial.print(F("Connecting to "));
    Serial.println(mySSID);
    // esp8266.connect([ssid], [psk]) connects the ESP8266
    // to a network.
    // On success the connect function returns a value >0
    // On fail, the function will either return:
    // -1: TIMEOUT - The library has a set 30s timeout
    // -3: FAIL - Couldn't connect to network.
    retVal = esp8266.connect(mySSID, myPSK);
    if (retVal < 0)
    { Serial.println(F("Error connecting"));
      errorLoop(retVal);
    }
  }
}

void displayConnectInfo()
{
  char connectedSSID[24];
  memset(connectedSSID, 0, 24);
  int retVal = esp8266.getAP(connectedSSID);
  if (retVal > 0)
  { Serial.print(F("Connected to: "));
    Serial.println(connectedSSID);
  }
  IPAddress myIP = esp8266.localIP();
  Serial.print(F("My IP: ")); Serial.println(myIP);
}

void serverSetup()
{ server.begin();
  Serial.print(F("Server started! Go to "));
  Serial.println(esp8266.localIP());
  Serial.println();
}

void serverDemo()
{
  ESP8266Client client = server.available(500);
  if (client) 
  {
    Serial.println(F("Client Connected!"));
    // an http request ends with a blank line
    boolean currentLineIsBlank = true;
    while (client.connected()) {
      if (client.available()) {
        char c = client.read();
        if (readString.length() < 100) { //read char by char HTTP request
              readString += c; //store characters to string
              }
              
        //if HTTP request has ended      
        if (c == '\n' && currentLineIsBlank) 
          {
          client.println("HTTP/1.1 200 OK");// send a standard http response header
          client.println("Content-Type: text/html");
          client.println();
          //=======================================================================
          cm1 = readString.substring(6,8);
          cm2 = readString.substring(8,11);
          Serial.print("readString = ");Serial.print(readString);Serial.println();          
          Serial.print("cm1 = ");Serial.print(cm1);Serial.println();
          Serial.print("cm2 = ");Serial.print(cm2);Serial.println();
          
          if(cm1 == "CM")
            {
             if(cm2 == "BZ1")
             { Serial.print("buzzer 1");Serial.println();
               readString = "";cm1 = "";cm2= "";client.stop(); // close connection:
             }
            }  
            break;
        }
      } // end if HTTP request has ended 
    } // while client connected
    delay(1); // give the web browser time to receive the data
   
    client.stop(); // close the connection:
    Serial.println(F("Client disconnected"));
  }
}

void errorLoop(int error)
{
  Serial.print(F("Error: ")); Serial.println(error);
  Serial.println(F("Looping forever."));
  for (;;)
    ;
}

```

---

<div class="post-metadata">

**Author:** ![paulvha](https://avatars.discourse-cdn.com/v4/letter/p/65b543/32.png) [@paulvha](https://community.sparkfun.com/u/paulvha)\
**Post date:** [July 6, 2019, 10:40am UTC](https://community.sparkfun.com/t/esp8266-http-request/37180/3 "2019-07-06T10:40:55Z")

</div>

Try to use the server.on(…, …) approach as in the AdvancedWebServer example of the ESP8266. it will enable to call a certain routine in your code depending on the extension of the URL.

---

<div class="post-metadata">

**Author:** ![dakota99](https://avatars.discourse-cdn.com/v4/letter/d/76d3ee/32.png) [@dakota99](https://community.sparkfun.com/u/dakota99)\
**Post date:** [July 6, 2019, 5:12pm UTC](https://community.sparkfun.com/t/esp8266-http-request/37180/4 "2019-07-06T17:12:02Z")

</div>

Hello thanks for your reply.

ESP8266WebServer.h seems a good solution.

But I can not make it work.

1. I use the Sparkfun ESP8266 WIFI shield on an Arduino Uno. First I have selected the board : Arduino Uno. But it seems it is not correct. I have to select : SparkFun ESP8266 Thing. Is it correct ?

2. The code below is compiled without error. But after upload to the board I get the following error :

File “C:/Users/Utilisateur/AppData/Local/Arduino15/packages/esp8266/hardware/esp8266/2.5.2/tools/esptool\esptool.py”, line 468, in connect

raise FatalError(‘Failed to connect to %s: %s’ % (self.CHIP\_NAME, last\_error))

esptool.FatalError: Failed to connect to ESP8266: Invalid head of packet (0x00)

Does someone knows what does that mean ?

Thanks for your help.

```auto
#include <ESP8266WiFi.h>
#include <ESP8266WebServer.h>

ESP8266WebServer server(80);
int ledPin = 16;
bool ledState = LOW;

void setup() {
   pinMode(ledPin, OUTPUT);
   Serial.begin(115200);
   WiFi.begin("",""); //Connect to the WiFi network
   while(WiFi.status()!= WL_CONNECTED){ //Wait for connection
      delay(500);
      Serial.println("Waiting to connect…");
   }
   Serial.print("IP address: ");
   Serial.println(WiFi.localIP()); //Print the local IP

   server.on("/on", turnOn); https://forum.sparkfun.com/viewtopic.php?f=121&t=50247https://forum.sparkfun.com/viewtopic.php?f=121&t=50247https://forum.sparkfun.com/viewtopic.php?f=121&t=50247https://forum.sparkfun.com/viewtopic.php?f=121&t=50247https://forum.sparkfun.com/viewtopic.php?f=121&t=50247https://forum.sparkfun.com/viewtopic.php?f=121&t=50247https://forum.sparkfun.com/viewtopic.php?f=121&t=50247https://forum.sparkfun.com/viewtopic.php?f=121&t=50247https://forum.sparkfun.com/viewtopic.php?f=121&t=50247 //Associate the handler function to the path
   server.on("/off", turnOff);     
   server.on("/toggle", toggle);   
   server.begin(); //Start the server
   Serial.println("Server listening");
}

void loop() {
server.handleClient();
}

void turnOn(){
ledState = HIGH;
digitalWrite(ledPin, ledState);
server.send(200, "text/plain", "LED on");
}

void turnOff(){
ledState = LOW;
digitalWrite(ledPin, ledState);
server.send(200, "text/plain", "LED off");
}

void toggle(){
ledState = !ledState;
digitalWrite(ledPin, ledState);
server.send(200, "text/plain", "LED toggled");
}

```

---

<div class="post-metadata">

**Author:** ![paulvha](https://avatars.discourse-cdn.com/v4/letter/p/65b543/32.png) [@paulvha](https://community.sparkfun.com/u/paulvha)\
**Post date:** [July 7, 2019, 7:37am UTC](https://community.sparkfun.com/t/esp8266-http-request/37180/5 "2019-07-07T07:37:20Z")

</div>

HI,

My error. Thought you were using an ESP8266 directly to the PC, but it is the shield on-top of an Arduino. So you have to select the correct Arduino .

More than a year ago I spend lots of time on this and have documented that on [https://github.com/paulvha/PVH\_ESP8266\_ … no\_Library](https://github.com/paulvha/PVH_ESP8266_AT_Arduino_Library)

Look at the pvh\_ESP8266\_Shield\_Server\_gpio or pvh\_ESP8266\_rfid\_reader examples. Focus on the server\_demo or Server\_Comms routines. Each use different approach to achieve the same : gpio uses the content of the message, RFID is using the URL parameters. There is lots of documentation in the extras folder about the different sketches and updated Sparkfun driver.

---

<div class="post-metadata">

**Author:** ![dakota99](https://avatars.discourse-cdn.com/v4/letter/d/76d3ee/32.png) [@dakota99](https://community.sparkfun.com/u/dakota99)\
**Post date:** [July 7, 2019, 6:03pm UTC](https://community.sparkfun.com/t/esp8266-http-request/37180/6 "2019-07-07T18:03:13Z")

</div>

Thanks Paul,

I have spent a lot of hours without result and I was considering to use NodeMCU.

But I will analyse the files you sent me and try to understand.

Thanks a lot for your help.