Gamepad Not Connecting to XRP Kit

Last year we were able to connect a gamepad to the XRP. This year we can not. The XRP board is having intermittent issues with it’s Websocket over BLE protocol that communicates the controller input to the XRP board for code execution purposes. Using both Blockly and Python programming the XRP only receives controller input after repeated restarts of the program, then returns to a no-communication state with the controller after a code restart. The problem persists with both prior and latest firmware versions, each with their respective XRPLib library versions installed on the board.

Latest Version tested - 2026.10.01 - Issue Persists

Double check/replace batteries in both. Can you get another BLE device to connect?

After uploading new firmware be sure to power the XRP off entirely and power it on, then reconnect it via usb…what version does it say it is running?

I’d recommend posting in https://xrp.discourse.group/, the main software developers are active there.