getting included project to run on at91sam9261

so i open it up today run it and get

source C:\gccfd\projects\gput91sam9261-ek-sdram.gdb
C:\gccfd\projects\gput91sam9261-ek-sdram.gdb:6: Error in sourced command file:
Cannot access memory at address 0xfffffc20
Configuring the master clock...
target remote localhost: 3333
0x00000000 in ?? ()
No line 581 in file "main.c".
No line 577 in file "main.c".
No line 588 in file "main.c".
No line 588 in file "main.c".
No line 588 in file "main.c".
monitor soft_reset_halt
requesting target halt and executing a soft reset
load
Loading section .fixed, size 0x1be0 lma 0x20000000
Loading section .postrelocate, size 0x6c lma 0x20001be0
Start address 0x20000000, load size 7244
Transfer rate: 76 KB/sec, 3622 bytes/write.
break main
Breakpoint 11 at 0x200004ac: file main.c, line 348.
continue
Unable to set 32 bit software breakpoint at address 200004ac

not too sure why that came up. this thing is driving me crazy. i have the 9260 dancing circles around itself, but i cant even get the 61 runnig