Hi all,
I’m planning to use two ROB-27478 gimbal motors as direct-drive wheel motors on a self-balancing robot. Each motor will run closed-loop FOC (SimpleFOC library) on its own SimpleFOCmini driver, powered from a 3S pack. The motor specs suit the application well, but neither the product page nor the datasheet documents the encoder side, so I have some questions before I order.
- Which AS5048A outputs are brought out to the encoder connector: SPI (CSn, CLK, MISO, MOSI), PWM, or both? Can you share the connector type, pin count and pinout?
- If the supplied cable carries PWM only, are the SPI signals accessible on the encoder PCB, either on pads or an alternate connector?
- Is the encoder board configured for a 3.3 V or a 5 V supply?
- The datasheet lists the encoder type as “AS5048A/AS5600”. Can you confirm that ROB-27478 always ships with the AS5048A?
- Has anyone at SparkFun run this motor closed-loop under FOC? Any notes on magnet alignment, air gap or field strength would help.
I have read in other forums of users of the same encoder (with similar motor - iPower GM3506) reporting PWM fails once the motor is commutating. Their problems disappeared after switching to SPI.