# ground planes and power

**URL:** <https://community.sparkfun.com/t/ground-planes-and-power/3445>\
**Category:** BatchPCB\
**Created:** [January 7, 2007, 3:51am UTC](https://community.sparkfun.com/t/ground-planes-and-power/3445 "2007-01-07T03:51:37Z")\
**Posts on this page:** 7\
**Page:** 1

<div class="post-metadata">

**Author:** ![yzf600](https://avatars.discourse-cdn.com/v4/letter/y/ce7236/32.png) [@yzf600](https://community.sparkfun.com/u/yzf600)\
**Post date:** [January 7, 2007, 3:51am UTC](https://community.sparkfun.com/t/ground-planes-and-power/3445/1 "2007-01-07T03:51:37Z")

</div>

I’ve seen almost every breakout board here on sparkfun has what I imagine is a ground plane on one or both sides. Perhaps there is a ground plane on one side and a power plane on the second side.

The reason I asked is because I’m having problems placing a ground plane with PCB. I got the ground plane all nice and neat in PCB, but the batch DRC bot showed the entire bottom layer as 1 copper rectangle shorted to all traces on the bottom. PCB shows the rectangle, but the traces are isolated from the ground plane by the 8mil spacing rules. gerbv shows the traces correctly as well. Just measuring the clearances now, gerbv shows only 5 mil spacing between the trace and the ground plane. Damn. Something else to fix.

What benefit do you get from having such planes on the same layer as the routes? Is there anything wrong with just routing power and ground a regular signal traces? Are regular signal traces not wide enough? In other words, what is the best practice? Both a ground plane and a power plane? Two ground planes with power routed as a fat trace?

BTW - My design is low power, using around 200mA max.

Any guidance would be much appreciated. Thanks.

---

<div class="post-metadata">

**Author:** ![Philba](https://avatars.discourse-cdn.com/v4/letter/p/ed655f/32.png) [@Philba](https://community.sparkfun.com/u/Philba)\
**Post date:** [January 7, 2007, 7:23am UTC](https://community.sparkfun.com/t/ground-planes-and-power/3445/2 "2007-01-07T07:23:07Z")

</div>

there are several different definitions in electronics but the one you are referring to is simply having an area of copper connected to ground. in 4 layer designs, an entire layer is often ground. it keeps the noise down. I’m sure more classically trained EEs will have a better explanation, though.

you don’t say what pcb cad sw you are using but it should have a way to change the isolation distance. in eagle its on the change menu item. I’d set it to a min of 10 mils though higher is going to increase the odds that your board comes back good.

---

<div class="post-metadata">

**Author:** ![hooziewhatsit](https://avatars.discourse-cdn.com/v4/letter/h/a9adbd/32.png) [@hooziewhatsit](https://community.sparkfun.com/u/hooziewhatsit)\
**Post date:** [January 8, 2007, 7:09am UTC](https://community.sparkfun.com/t/ground-planes-and-power/3445/3 "2007-01-08T07:09:24Z")

</div>

email them and ask about it.

I recently sent in a design that had power planes on both sides (with curves). The .jpg in the reply email showed everything messed up. Apparently there’s a bug in the generation of the .jpg, but the board _should_ turn out just fine.

-Dave

---

<div class="post-metadata">

**Author:** ![busonerd](https://avatars.discourse-cdn.com/v4/letter/b/958977/32.png) [@busonerd](https://community.sparkfun.com/u/busonerd)\
**Post date:** [January 8, 2007, 5:22pm UTC](https://community.sparkfun.com/t/ground-planes-and-power/3445/4 "2007-01-08T17:22:58Z")

</div>

There are two issues I know of - 1 is that ‘clear’ polygons are drawn as filled - which is probably what the first poster is experiencing. That’ll get fixed when I have time to rewrite the polygon generation engine.

The second is incorrect curve rendering - which I’ve been meaning to get around to for a while - and might get to today. Thats what hit your design Dave.

Cheers,

–David Carne

---

<div class="post-metadata">

**Author:** ![bigglez](https://avatars.discourse-cdn.com/v4/letter/b/ac91a4/32.png) [@bigglez](https://community.sparkfun.com/u/bigglez)\
**Post date:** [January 8, 2007, 6:35pm UTC](https://community.sparkfun.com/t/ground-planes-and-power/3445/5 "2007-01-08T18:35:23Z")

</div>

> yzf600:  
> What benefit do you get from having such planes on the same layer as the routes? Is there anything wrong with just routing power and ground a regular signal traces? Are regular signal traces not wide enough? In other words, what is the best practice? Both a ground plane and a power plane? Two ground planes with power routed as a fat trace?

Greetings (no name supplied),

There are cases where a ground plane is required as the PCB is a component in a critical circuit. Typically, these are RF designs, where circuits must resonate at the correct frequency, and/or carry RF power efficiently (without losses). In very low level circuits (sensors, high resolution A2D and D2A converters, measuring instruments, transducer preamplifiers, etc.) the ground plane acts as a shield or barrier to exclude external electrical noise.

In the days of combinational logic built on bipolar IC processes (DTL, TTL, ECL) a lot of power was consumed and switching caused large spikes on both the power and ground circuits. Ground (and power) planes were added to reduce the inductance of the supply and ground, effectively increasing the noise immunity.

More recent designs using lower power circuits (battery operation in particular), the use of mixed-signal ICs (analog and digital on the same die) and increasing use of RF communications has made the use of a PCB ground plane attractive.

Some circuits fail to operate, or have reduced performance, on a ground plane due to increased capacitance loading and interference from noisy power and ground lines coupling into high impedance and high gain stages. In particular, any device that uses a crystal, ceramic resonator, or NFB (negative feedback) will require that ground planes are removed in critical areas.

It’s not the copper resistance that causes the problem, although high power circuits benefit from “fat” traces or extra weight copper, but the inductance. Small width traces, or traces that run parallel (even on opposite sides of the PCB) will exhibit greater noise, and possibly coupling between the traces. A ground plane can eliminate this problem.

On single and two layer PCBs its a good idea to flood the unused areas to form a ground plane (but not in the areas noted above). Its considered bad practice to leave islands (or orphans) of ground plane that are not electrically connected to ground. Its also possible to section a PCB layer to form power planes of different voltages or power and ground. or two separate ground to isolate analog and digital circuits on the same PCB.

PCBs can be effective without any planes, by routing the power and ground as ‘signal’ traces. There’s a few rules to making this work the first time, mostly its common sense. If in doubt think of the traces as small resistors. What will happen to the circuits if voltage is lossed in each segment of the trace? Will it reduce the available voltage at the end of the line furthest from the power source? Will a heavy load cause voltage drops on the power traces that effect other curcits? Remember that current must return to the power source, so similar losses occur in the ground traces to those in the power traces.

Allowing space to place wider traces for power and ground compared with signals (many of which carry less than one percent of the total current in a given circuit) will help.

Advances in IC processing produces finer feature size (the smallest element in the silicon), but operating voltages must be reduced due to lower breakdown voltages. This leads to greater current for a given processing performance, and makes power design, distribution, and decoupling quite difficult. Many large scale digital devices now use less than one volt for their core, less than three volts for their IO, and consume tens of watts. This translates to tens of amps, which requires fat traces to reduce the I2R losses. Further, the switching regulators used to power these circuits have very large high speed circulating currents that require very careful PCB design and layout.

In my experience, having worked on high speed analog and digital systems, it may take more than half a dozen PCB revisions to get it right. These are just that - PCB layout changes. Not architecture or circuit changes, or substitution of different packages and devices, just placement of traces and scupturing of the ground and power planes, and addition or subtraction of vias.

For BatchPCB level hobby projects adding a power plane may have a very small effect. Critical circuits will likely have hints in their data sheets. I think ground planes are attractive, and I’ve found out the hard way that without “thermals” (breaks around pads and vias on the ground plane) it can be very hard to get good soldering.

Power planes and ground planes are typically not allowed in inner layers of multi-layer boards for a variety of PCB production reasons, and I think they are banded in the new BatchPCB four layer service (can someone confirm this - I hate to spead false info). Also, I wonder if blind vias are allowed (ones that connect inner layers without removing route area on the outer layers?

Comments Welcome!

---

<div class="post-metadata">

**Author:** ![busonerd](https://avatars.discourse-cdn.com/v4/letter/b/958977/32.png) [@busonerd](https://community.sparkfun.com/u/busonerd)\
**Post date:** [January 8, 2007, 9:07pm UTC](https://community.sparkfun.com/t/ground-planes-and-power/3445/6 "2007-01-08T21:07:57Z")

</div>

> Power planes and ground planes are typically not allowed in inner layers of multi-layer boards for a variety of PCB production reasons

Er... uh.... no?

The most common place for the PCB + GND plane on a multilayer board is on the internal layers, simply because SMT parts don’t mix well with with planes.

A typical 4 layer stackup is S/G/P/S - and a 6 layer one I’m fond of is S/G/P/S/G/S. I’ve run both stackups before in production quantities. The ONLY restriction on planes I know of are “imbalanced” stackups - where all the planes are concentrated towards one side of the stack. That can create problems when reflowing boards as the board expands unevenly - leading to warping and sometimes delamination.

We’re quite happy to run a 4 layer board with planes inside.

Cheers,

–David Carne

---

<div class="post-metadata">

**Author:** ![bigglez](https://avatars.discourse-cdn.com/v4/letter/b/ac91a4/32.png) [@bigglez](https://community.sparkfun.com/u/bigglez)\
**Post date:** [January 8, 2007, 9:59pm UTC](https://community.sparkfun.com/t/ground-planes-and-power/3445/7 "2007-01-08T21:59:49Z")

</div>

> busonerd:
> 
> > Power planes and ground planes are typically not allowed in inner layers of multi-layer boards for a variety of PCB production reasons
> 
> Er... uh.... no?

David,

I stand corrected. Good news, about the inner planes.

Comments Welcome!