# Having issues with openscale board

**URL:** <https://community.sparkfun.com/t/having-issues-with-openscale-board/69729>\
**Category:** Input Devices\
**Created:** [October 12, 2026, 8:55pm UTC](https://community.sparkfun.com/t/having-issues-with-openscale-board/69729 "2026-10-12T20:55:10Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![Zjones](https://avatars.discourse-cdn.com/v4/letter/z/bcef8e/32.png) [@Zjones](https://community.sparkfun.com/u/Zjones)\
**Post date:** [October 12, 2026, 8:55pm UTC](https://community.sparkfun.com/t/having-issues-with-openscale-board/69729/1 "2026-10-12T20:55:10Z")

</div>

Hello,

I’m using an Arduino Uno with input from a open scale board (13261). I’m using a 13332 sparkfun load cell. I’ve burned up 2 open scale boards. They both worked for a bit then stopped working. When checking the open scale board by plugging into my computer usb they started smoking from the same stop. I’m trying a 3rd board now. It seems to be working because the LED is flashing. The load cell now seems to be damaged. Anyone have any ideas what I have done wrong? I would say it’s not wiring since they both worked for a bit but could be wrong. The Arduino is still functioning fine. Below is how I have everything hooked up:

 ![image](https://canada1.discourse-cdn.com/sparkfun/original/2X/b/b097611b9cd3f89764760f21b9bf32e0508b28ba.jpeg)

This is my first experience with an open scale card.

---

<div class="post-metadata">

**Author:** ![TS-Russell](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/ts-russell/32/6092_2.png) [@TS-Russell](https://community.sparkfun.com/u/TS-Russell)\
**Post date:** [October 12, 2026, 11:05pm UTC](https://community.sparkfun.com/t/having-issues-with-openscale-board/69729/2 "2026-10-12T23:05:31Z")

</div>

Can you share a photo of the soldering/wiring going from the Openscale to the Arduino? Be sure to use the 5v pin to power the Openscale, not VIN

Also double-check that the screw-hole terminal wires are not touching one another/shorting. You can measure the load cell’s bridge resistance with a meter: E+ to E- and A+ to A-. A TAL220-type cell should read a few hundred ohms, with no shorts

To isolate variables you can try powering the openscale over usb without the arduino or load cell attached…if it stays cool (no overheating/smoke) you can then try adding the load cell…if that works fine you can then go back to all 3 (add arduino back)