Well, I finally brought out the big guns and dusted off my old Hitachi O-scope (20MHz) that I bought out of college in 1984
and took some screen shots of what I saw on the scope. Very interesting.
First, I checked the TX data in line to see if I could see the Linx encoding wave. Sure enough. I got a completely continuous (locked) encoding pattern. See this picture of the O-scope image: http://flash.360vl.com/~lcox/breadboard … ataOut.jpg The scope is showing about 5 volts per major graduation so this looks very TTL-ish as I would expect. Again, this reading was taken on the Data Out side of the encoder that goes to the TX data line.
Secondly, I checked the digital data port on the RX side to see if I could see a corresponding wave. It’s also obvious that the encoding is making it through the RF, albeit, by the time it goes into the Linx Decoder, the wave form amplitudes are not pure TTL any more. Here’s a screen of the O-scope on the Data output of the Receiver (Data input to the decoder.): http://flash.360vl.com/~lcox/breadboard … ata-In.jpg. Notice the TX and RX patterns correspond but the RX side is not at 0-5V like the TX side is…it looks more like 2.5-5v transitions.
Anyway, I’m not sure what to do about this at this point. It’s clear the encoding is making it across the RF link but is different enough that it’s not like the TX encoder output is connected to the RX decoder input - that worked, but going across the RF doesn’t and it’s obviously due to the difference in the wave form.
I don’t know if it’s due to the level changing that occurs coming out of the RX or some other factor. It seems like the wave is somewhat slower as I can see the edges on the RX side but on the TX side, I could only see the levels and not the edges. Don’t know if that’s meaningful, but just an observation based on these pictures.
Any ideas to try next?