To polish off my part of this thread and followup on what I found:
Bruce of Rentron sent me a new encoder/decoder (you’ll need to contact Rentron to learn more about them.) The ones I got I think were experimental but hopefully close to production - The encoder had a gold dot on it and the decoder had a silver dot on it - that was all there was for a marking on the chips.
These chips are pin-for-pin compatible with the Linx encoder/decoder.
Once I breadboarded them up, they worked flawlessly for what I was planning and they worked fine over the 2400bps low-grade 434 RF radios I got from Sparkfun.
I created two protoboards - a TX and an RX. The TX board has 4 photointerrupter switches that feed D0-D3 of the encoder. The encoder’s data out, of course, goes to the data pin of the transmitter.
On the flip side, I wired digital data pin of the receiver to the Data In pin of the decoder. Then strung 4 LEDs off D0-D3.
With this setup, whenever the photointerrupter was blocked, I got a solid LED light on the RX side. This was exactly the behavior I was looking for and couldn’t get with the Linx encoders.
Here are the pictures of my latest protoboards.
Transmitter:
http://flash.360vl.com/~lcox/breadboard/Transmitter.jpg
Receiver:
http://flash.360vl.com/~lcox/breadboard/Receiver.jpg
Each protoboard has a 434 antenna I bought from Rentron. I’ve tested these on the bench maybe a foot apart all the way up to maybe 40 feet. One test I did between floors where the two ends were probably 25 feet apart, but separated by a floor.
It was all working very well thanks to the new encoders from Rentron.
Bruce, thanks again for going above and beyond the call of duty and working on this over Thanksgiving weekend to diagnose the issues with the newer radios.
Hopefully, this exercise will be of use to others.