So I’ve been building a system based solely around RP Pico’s. One RP2350 W is the main server displaying these web pages.
All communication via WiFi and no MQTT hub required. The whole system consists of
- Pico2W handling the webserver and controls
- the second CPU in the Pico 2W handling an LCD display
- 2 temperature sensors (living room and garage)
- 1 temp/humidity/pressure sensor in lanai
- 2 Shelly plugs controlling lights
- 1 Kauf bulb over the entry way with flashy red/white/blue every couple minutes
- 1 PIR sensor on PicoW which controls a Kasa plug lights in a dark garage (my wife thinks this is the best part)
- Ambient light sensor will turn on a selected light when dark during daytime storms
- Control of lights based on sunset or time
- Cloudflare tunnel to access from anywhere
- PIR sensor with RP2040 controlling light via a Kasa plug.
- a soil moisture sensor powered from a canabalized solar light
As the RP2350 has 2 CPUs, the idle one was setup to drive a display (necessary, not really just blinking light factor)
So what software is involved -
- html and css stored on the Pico 2W
- either BASIC or C to handle the sensor or hub functions
- low level C for BASIC firmware version
- C/ BASIC compilers on PC/Linux/RPi
One key to the interactive webpages is /?cgi functions that call underlying routines or display/set variables.
Also a <?web construct that executes routines in the underlying code, or does simple if statements.
And a wprintf in C or BASIC that generates html content for the webpages.
Drop me a line for a link to ALL the sources.
Also some of the enclosures (from Amazon or Pi shop – maybe someday I’ll try my hand at 3D printing). Double sticky taped to USB charger – temp sensors deliberitly outside the boxes, or velcro so I can update them. The PIR sensor was triggered by the RP2040W so had to be seperate.