I really appreciate your thorough reply. I certainly took the time to read the entire guide, everything on the Robertsonics site and all the forum posts I could find. I didn’t find the information I needed anywhere.
I solved this problem yesterday. I got an email from Robertsonics that reiterated the newer firmware version available. I made the bad assumption that because I bought a board recently I would get the latest firmware. That apparently wasn’t the case. I have included my log below, but basically I was able to accomplish Trigger 1 plays a random track every time it is triggered and stops at the end of the track. The track can be interrupted by triggering again. The track does not loop if Trigger 1 remains HIGH/active.
INI file:
#TRIG 01, 2, 0
All files are named according to the protocol, 001.mp3, 002.mp3, etc.
As you said, the #RAND wasn’t necessary. The STOP command on pin 18 also wasn’t necessary. I just have a switch wired to pin 1 and ground.
The latest firmware can be found at the bottom of the Robertsonics website:
https://www.robertsonics.com/downloads/
Log:
***First attempt:
#RAND
#TRIG 01, 2, 0
#TRIG 18, 5, 0
Tracks named with 001, 002, etc.
Formatted card, added songs one at a time, in order, ini first
–Some files were WAVs; trigger not activating (no LED indicator when activated); no sound output
***Second attempt:
#RAND
Tracks named with 001, 002, etc.
Formatted card, added songs one at a time, in order, ini first
–Trigger 01 works; plays track named 001 every time; no random; audio stops after 001 is played
***Third attempt:
#TRIG 01, 2, 0
Tracks named with 001, 002, etc.
Modified ini while on the card; left files on card (no format)
–Trigger 01 works; playes track 001 every time; no random; audio stops after 001 is played; no loop, even if trigger is constant on
***Fourth attempt:
Downloaded and updated firmware on board.
Repeated first attempt exactly with new firmware
–Trigger 01 works; plays track 001 every time; no random; no restart lockout - track restarts every time trigger is activated; audio stops after 001 is played
***Fifth attempt:
Repeated second attempt with new firmware
–Exact same as fourth attempt
***Sixth attempt:
Repeated third attempt exactly with new firmware
#TRIG 01, 2, 0
All tracks named with 001*.mp3, etc.
--Works! Trigger 01 plays a random track every time it is activated; audio stops when track is complete, even if trigger is active; no restart lockout; interruption of track plays next random track (sometimes repeats same “random” track order if trigger is activated too soon - less than 1 second)