ID-12 module testing

Madeleine, thanks so much for your help

I’ve recreated this circuit on a breadboard and hooked it up to a (measured) 5VDC power supply.

http://www.raymondblum.net/img/id12.jpg

(The ID12 is soldered into the Sparkfun breakout board)

The resistor is 1K, from pin 10 to the LED

The following pins are connected:

1 - GND

2 - +5VDC

7 - GND

10 - 1K - LED - GND

11 - +5VDC

When I switch the power on, I see a brief flash on the LED.

My test is simple enough, I have 2 HID cards (my building security cards from work). I pass either of them over the ID12 module, between a half inch to an inch from the module surface. No LED activity to be seen.

Is there anything wrong with this circuit that anyone can spot or do I have a defective/damaged module?

Thanks

–Raymond

Are you sure your cards are the correct type of RFID cards? They need to be 125KHz with this module.

They need to be 125khz, and a particular protocol / encoding. The ones from SparkFun Electronics definitely work.

Cheers,

–David Carne