Hi InPlay Support Team,
can you please connect me with any technical expert to help me to resolve this problem?
We are evaluating the IN100 NanoBeacon for a beacon application involving an I2C temperature sensor (TMP110), with the intent to move to high-volume production if the evaluation is successful.
─── Issue Summary ───────────────────────────────────
During OTP burn, the NanoBeacon Config Tool fails at 8% progress with the following error:
“Failed to write eFuse, maybe it is VDDQQ power issue!”
RAM mode works correctly — all advertising data functioning as expected.hence i2c test not support in RAM mode to test I2c we burn. The failure occurs exclusively during the Burn/Program step.
─── Hardware Setup ──────────────────────────────────
Programmer : PL2303 USB-to-UART (TTL) module
Connections:
PL2303 3.3V ── NanoBeacon VCC
PL2303 GND ── NanoBeacon GND
PL2303 TX ── NanoBeacon RX
PL2303 RX ── NanoBeacon TX
using dev Board form SmartElex hence quick available at our location.
Board under test : SparkFun NanoBeacon Board - IN100
─── Power Supply Attempts ───────────────────────────
We have attempted burn with two separate power sources with two board — both result in the same error at 8%:
Attempt 1 : CR1225 coin cell (3V) via onboard battery holder
Attempt 2 : external power by nordic PPK2 (external regulated supply)
In both cases, TX/RX communication is stable and RAM mode executes without any issue.
─── Software ────────────────────────────────────────
Config Tool version : NanoBeaconConfigToolMpTool_V3.3.4B
OS : Windows
─── Attachments ─────────────────────────────────────
- config file
config.txt (5.5 KB)
2. GUI error screenshot
─── Questions ───────────────────────────────────────
1. What is the minimum VCC current capability required specifically
during eFuse/OTP programming? Is there a VDDQQ specification
separate from the normal operating VCC?
2 . Are there any known issues with OTP burn on the SmartElex
NanoBeacon board variant at this tool version?
3. any pre-process before burn with e-fuse?
Any guidance or troubleshooting steps would be greatly appreciated. as we have one more fresh board left to try any. We are keen to resolve this quickly as this evaluation directly influences
our volume procurement decision.
(NOTE: gui downloaded from INplay website(NanoBeaconConfigToolMpTool_V3.2.29) and then updated by prompt on gui launch to ask for update to V3.3.4B.
Best regards,
Jay.
shipmentia(WaveInnova)