# interfacing with nRF24L01 chip antenna

**URL:** <https://community.sparkfun.com/t/interfacing-with-nrf24l01-chip-antenna/8565>\
**Category:** Wireless & IoT\
**Created:** [September 24, 2008, 3:55pm UTC](https://community.sparkfun.com/t/interfacing-with-nrf24l01-chip-antenna/8565 "2008-09-24T15:55:23Z")\
**Posts on this page:** 4\
**Page:** 1

<div class="post-metadata">

**Author:** ![flame79boy](https://avatars.discourse-cdn.com/v4/letter/f/d26b3c/32.png) [@flame79boy](https://community.sparkfun.com/u/flame79boy)\
**Post date:** [September 24, 2008, 3:55pm UTC](https://community.sparkfun.com/t/interfacing-with-nrf24l01-chip-antenna/8565/1 "2008-09-24T15:55:23Z")

</div>

i am trying to interface PIC16F88 with nRF24L01 with chip antenna board. I am struggling to communicate with the device. Does anyone know what you have to do, to read values from nRF24L01? i am really struggling to talk to the device over SPI.

Any insights would be greatly appreciated.

A.

---

<div class="post-metadata">

**Author:** ![leon\_heller](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/leon_heller/32/7602_2.png) [@leon\_heller](https://community.sparkfun.com/u/leon_heller)\
**Post date:** [September 24, 2008, 5:09pm UTC](https://community.sparkfun.com/t/interfacing-with-nrf24l01-chip-antenna/8565/2 "2008-09-24T17:09:04Z")

</div>

Here’s some code of mine:

```auto
; ***************************************************************
;Test.asm
;Tx/Rx test program for MiRF V2
;MCU: PIC16F88
;uses hardware 16F88 SSP module (hardware SPI)
;
;user interface
;LED - RB5, output (pin 11)
;PB - RA1, input (pin 18)
;
;nRF24L01 connections to 16F88
;
;IRQ - RA0, input (pin 17)
;CE - RB0, output (pin 6)
;MISO/SDI	- RB1, input (pin 7)
;MOSI/SDO	- RB2, ouput (pin 8)
;CSN - RB3, output (pin 9)
;SCK - RB4, output (pin 10)
; ***************************************************************

	errorlevel -302

#define IRQ 0
#define	MISO 1
#define MOSI 2
#define	SCK 4
#define	CSN 3
#define	CE 0
#define	LED 5
#define PB 1

;defines for software SPI

#define SPI_SCK 4
#define SPI_SO 2
#define SPI_SI 1

#include	<p16f88.inc>

	CBLOCK 0x20
	scrA:	1	; scratch pad	0x20
	scrB:	1
	count
	RXDATA
	TXDATA
	status
	data_0
	data_1
	data_2
	data_3
	data_4
	ENDC

	org 0

	nop

; **************************************************************
;main program
; **************************************************************
	call	init
	banksel	PORTB
	call	flash_led

zzz:
	bcf PORTB,CSN ;CSN low
	call	short_dly
	
	movlw	0x10 ;send command (read configuration)
	movwf	TXDATA ;put in TXDATA
	call	spi_send_read	;send it
	call	short_dly

	call	spi_send_read
	movfw	RXDATA ;status is first byte received
	movwf	status ;save it
	call	short_dly

	call	spi_send_read
	movfw	RXDATA
	movwf	data_0
	call	short_dly

	call	spi_send_read
	movfw	RXDATA
	movwf	data_1

	call	spi_send_read
	movfw	RXDATA
	movwf	data_2

	call	spi_send_read
	movfw	RXDATA
	movwf	data_3

	call	spi_send_read
	movfw	RXDATA
	movwf	data_4

	nop
	bsf PORTB,CSN ;CSN high
	nop
	goto	zzz

stop:
	goto	stop

aaa:

	BANKSEL	SSPSTAT
LOOP: 	
	BTFSS SSPSTAT, BF ;Has data been received (transmit complete)?
	GOTO LOOP ;No
	BCF STATUS, RP0 ;Specify Bank0
	MOVF SSPBUF, W ;W reg = contents of SSPBUF
	MOVWF RXDATA ;Save in user RAM, if data is meaningful
	MOVF TXDATA, W ;W reg = contents of TXDATA
	MOVWF SSPBUF ;New data to xmit

	goto	aaa

spi_send_read:
	banksel	PORTB
	bcf PORTB,SPI_SCK	;SCK low
	movfw	TXDATA
	movlw	8 ;8 bits to send
	movwf	count
sp1_1:
	rlf TXDATA,f ;MS bit in C
	btfss	STATUS,C ;C = 0?		
	goto	spi_2 ;no, jump
	bsf PORTB,SPI_SO	;yes, output one
	goto	spi_3
spi_2:
	bcf PORTB,SPI_SO	;output zero
spi_3:
	btfsc	PORTB,SPI_SI	;SPI_SI input low?
	goto	spi_4 ;no, jump
	bcf STATUS,C ;yes, clear carry bit
	goto	spi_5
spi_4:
	bsf STATUS,C ;set carry bit
spi_5:
	rlf RXDATA,f ;rotate RXDATA left
	bsf PORTB,SPI_SCK	;SCK high to latch bit
	decfsz	count,f ;count = 0?
	goto	sp1_1 ;no, loop back
	return ;yes, return

; ***************************************************************
;initialisation
; ***************************************************************
init:

	;oscillator setup
	BANKSEL	OSCCON
	MOVLW	0x70 ; 8 MHz int. RC osc.
	MOVWF	OSCCON

WAIT1:
	BTFSS	OSCCON,2	; wait until freq. is stable
	GOTO	WAIT1

	;I/O setup
	BANKSEL PORTA ; select bank of PORTA
	CLRF PORTA ; Initialize ports by
	CLRF	PORTB ; clearing output data latches
	BANKSEL	ANSEL ; Select Bank of ANSEL
	MOVLW	0x00 ; Configure all pins
	MOVWF	ANSEL ; as digital
	BANKSEL TRISB
	MOVLW	0x02 ; configure PORTB I/O (00000010)
	MOVWF	TRISB	
	MOVLW	0x01 ;configure PORTA I/O (00000001)
	MOVWF	TRISA
	banksel	PORTB
	bsf PORTB,CSN	;CSN high
	bcf PORTB,CE	;CE low

	return

	;SPI setup
	BANKSEL	SSPSTAT
	MOVLW	0x40 ;SPI master mode (01000000)
	MOVWF	SSPSTAT
	MOVLW	0x32 ;enable SSP for SPI master mode, clock = OSC/64 (00110010)
	MOVWF	SSPCON

	RETURN

; ******************************************************************
;flash LED five times
; ******************************************************************
flash_led
	movlw	5
	movwf	count
flash1:
	BSF PORTB,LED	;toggle LED
	call	dly
	BCF PORTB,LED
	call	dly
	decfsz	count,f
	goto	flash1
	return

; ****************************************************************
;transmit configuration
; ****************************************************************
Tx_config:
	banksel	PORTA
	clrf	PORTA
	movlw	0x38
	movwf	TRISA
	bcf	PORTA,CE	;set config mode (CE = 0, CSN = 1)
	nop
	bsf	PORTA,CSN
	call	dly
	;send 24 bit configuration word 001000110100111000000100 (0x234E04) MS bit first
	movlw	0x23
	call	put_byte
	movlw	0x4E
	call	put_byte
	movlw	0x04
	call	put_byte
	call	dly
	banksel	PORTA
	bcf	PORTA,CE
	nop
	bsf	PORTA,CSN	;configuration enabled on falling edge of CSN
	return

; ******************************************************************
;receive configuration
; ******************************************************************
Rx_config:
	banksel	PORTA
	clrw
	movfw	PORTA ;all bits low
	movlw	0x38 ;DATA1, DR1 output
	movfw	TRISA
	banksel	PORTA
	bcf	PORTA,CE	;set config mode (CE = 0. CS = 1)
	bsf	PORTA,CSN
	call	dly
	;send 24 bit configuration word 001000110100111000000101 (0x234E05) MS bit first
	movlw	0x23
	call	put_byte
	movlw	0x4E
	call	put_byte
	movlw	0x05
	call	put_byte
	banksel	PORTA
	bcf	PORTA,CE
	nop
	bcf	PORTA,CSN
	clrw
	movwf	PORTA
	movlw	0x3A ;DATA1 muse be input
	movwf	TRISA
	bcf	PORTA,CE
	nop
	bsf	PORTA,CSN
	return

; *****************************************************************************
;transmit data
; *****************************************************************************
Tx_data:
	banksel	PORTA
	bsf	PORTA,CE	;power up RF front end (CE = 1)
	call	dly
	movlw	0xE7 ;RF address 11100111 (0xE7)
	call	put_byte	;clock in address
	movlw	0x11 ;send four data bytes (0x11223344)
	call	put_byte
	movlw	0x22
	call	put_byte
	movlw	0x33
	call	put_byte
	movlw	0x44
	call	put_byte
	bcf	PORTA,CE	;start transmission (CE = 0)
	return

; ****************************************************************************
;receive data
; ****************************************************************************
Rx_data:
	banksel	PORTA
	bcf	PORTA,CE	;power down RF front end
	clrf	data_0 ;zero buffers so that we can ensure that
	clrf	data_1 ;correct date is being received
	clrf	data_2
	clrf	data_3
	call	get_byte	;receive four bytes and save in buffer
	movwf	data_0
	call	get_byte
	movwf	data_1
	call	get_byte
	movwf	data_2
	call	get_byte
	movwf	data_3
	bsf PORTA,CE	;power up RF front end
	return

; ***************************************************************************
;send byte to nRF24L01 (MS bit first)
;byte in WREG
; ***************************************************************************
put_byte:
	banksel	PORTA
	movwf	scrA	;save byte
	movlw	8	;initialise bit counter
	movwf	count
put_1:
	btfsc	scrA,7	;bit 7 = 0?
	goto	put_2	;no, jump
	bcf PORTA,MOSI	;clear DATA
	nop
	bsf PORTA,SCK	;clock it
	nop
	bcf PORTA,SCK
	goto	put_3
put_2:
	bsf PORTA,MOSI	;set DATA
	nop
	bsf PORTA,SCK	;clock it
	nop
	bcf PORTA,SCK
put_3:
	rlf scrA,f ;left shift for next bit
	decfsz	count,f ;more bits?
	goto	put_1 ;yes, loop back
	return ;no, return			

; ***************************************************************************
;get byte from nRF24L01 (MS bit first) by clocking in data from MISO
;byte returned in WREG
; ***************************************************************************
get_byte:
	banksel	PORTA
	movlw	8 ;initialise bit counter
	movwf	count
get_1:
	btfsc	PORTA,MISO	;data = 1?
	goto	get_2		
	bcf scrA,0 ;no, clear MS bit
	goto	get_3
get_2:
	bsf scrA,0 ;Yes, set MS bit
get_3:
	bsf PORTA,SCK
	nop
	bcf PORTA,SCK
	rlf scrA,f ;left shift for next bit
	decfsz	count,f ;more bits?
	goto	get_1 ;no, loop back
	movfw	scrA ;return with byte in WREG
	return

; **************************************************************************
;delay routine
; **************************************************************************
dly:
	movlw	0xFF
	movwf	scrB
dly_1
	movlw	0xFF                        
	movwf	scrA                          
dly_2:	
	decfsz	scrA, F                    
	goto	dly_2
	decfsz	scrB,F
	goto	dly_1                          
	return
	

short_dly:
	movlw	0x0F                        
	movwf	scrA                          
short_1:	
	decfsz	scrA, F                    
	goto	dly_2
	decfsz	scrB,F
	return

	end

```

Leon

---

<div class="post-metadata">

**Author:** ![flame79boy](https://avatars.discourse-cdn.com/v4/letter/f/d26b3c/32.png) [@flame79boy](https://community.sparkfun.com/u/flame79boy)\
**Post date:** [September 26, 2008, 3:46pm UTC](https://community.sparkfun.com/t/interfacing-with-nrf24l01-chip-antenna/8565/3 "2008-09-26T15:46:41Z")

</div>

hi leon,

thanks for your code, it was very modular and uses software SPI routines.

---

<div class="post-metadata">

**Author:** ![leon\_heller](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/leon_heller/32/7602_2.png) [@leon\_heller](https://community.sparkfun.com/u/leon_heller)\
**Post date:** [September 26, 2008, 4:02pm UTC](https://community.sparkfun.com/t/interfacing-with-nrf24l01-chip-antenna/8565/4 "2008-09-26T16:02:31Z")

</div>

I converted the SFE C code (it had software SPI) into assembler. I ought to update it to use hardware SPI. I’ve done that with my C code for the 18F4520 and MiRF V2.

Leon