# Is it possible to get the position at 10 Hz using the "SparkFun GPS-RTK-SMA Kit"?

**URL:** <https://community.sparkfun.com/t/is-it-possible-to-get-the-position-at-10-hz-using-the-sparkfun-gps-rtk-sma-kit/44264>\
**Category:** Development Boards\
**Created:** [July 27, 2022, 3:10am UTC](https://community.sparkfun.com/t/is-it-possible-to-get-the-position-at-10-hz-using-the-sparkfun-gps-rtk-sma-kit/44264 "2022-07-27T03:10:10Z")\
**Posts on this page:** 1\
**Page:** 1

<div class="post-metadata">

**Author:** ![Ryo](https://avatars.discourse-cdn.com/v4/letter/r/a587f6/32.png) [@Ryo](https://community.sparkfun.com/u/Ryo)\
**Post date:** [July 27, 2022, 3:10am UTC](https://community.sparkfun.com/t/is-it-possible-to-get-the-position-at-10-hz-using-the-sparkfun-gps-rtk-sma-kit/44264/1 "2022-07-27T03:10:10Z")

</div>

Hi,

I plan to use “SparkFun GPS-RTK-SMA Kit” to get the drone’s position(10Hz).

For this purpose, we are planning to use a set for the base station on the ground and a set for the rover station on the drone.

We assume that the maximum distance between the rover and the base is about 400 meters, and the measurements are taken in open area.

Now I have two questions.

**First** , the rover need to connect PC or don’t. Because there are no space to put the PC on the drone.

**Second** , is there a device that is just the right means of communications between the base and the rover needed for RTK positioning?

Thank you! 😃 😃