My goal is to have a setup where a torch acts as a base, and it sends corrections to a drone via NTRIP and another torch that will be on a survey pole for measuring roads.
Let me describe my setup:
- I have one torch setup in Base Caster mode and LoRa enabled;
- I have another torch in rover mode and LoRa enabled;
- I have a drone (the Autel Evo2 Pro v3 with RTK antenna), I connect to the wifi of the Base Caster Torch, and am able to log in and connect to the Access Point of the torch
Now here is what happens:
- If I leave the GNSS options at their defaults (all constellations, default RTCM messages enabled at default rates) on the base, I get a float but not a fix, the stddev starts at around 300 cm, sort of gradually decreases to about 150 cm, then goes back to 300 cm. and of course the rover torch gets a fix no problem.
- If I turn off Beidou and QZSS and hit the “low bandwidth” button on the base in the RTCM messages menu to get the lower frequency transmission of messages, I am able to get a fix on both the drone and the torch acting as a rover.
- If I turn off Beidou and QZSS but leave the RTCM rates and messages at their defaults, The drone stays at float and the torch rover gets a fix. Now I did not leave the torches running for too long because I was in a hurry, so is it possible that if i left it for longer it could get fix? I need to see.
I am trying to figure out what specifically is keeping the drone from getting a fix. I have two possible ideas, let me know if you have others:
- The drone’s manual indicates it only uses Gallileo, GLONASS, GPS and Beidou, I am wondering if QZSS is messing with how the drone calculates an rtk position or something
- There is a bandwidth issue somewhere, and since the Rover Torch was able to get a fix with all of the default settings enabled on the base, then the issue would have to be on the drone’s side, and I need to figure out what that is. Does anyone have an idea on how to determine the bandwidth that is going between the Drone and torch? or what messages are making it through?