hi people,
i have the same problem, and im struggling with this since long, i consulted assitance from olimex but that did not help either.
When i plug in the OLIMEX ARM-USB_OCD (not tiny) windows is first of all not asking for any driver installing it byself as a USB Combined Device, and the LED is lighting red on the ARM-USB_OCD. Then i try to install it by myself, i show windows the location as “C:\GCCFD\Olimex OpenOCD Driver” which came with the OLIMEX-GCCFD-190207.exe installer. This setup supplied by olimex is telling at the end of the installation that the driver has to be installed 3 times “and that it is not a joke”. In the driver folder there are “FTDIBUS.INF” and “FTDIPORT.INF” files. Ok, then i show windows this folder but windows is telling me that it cant find a better driver than the one installed now(USB Combined Device). So i try it with “Dont look, i will choose the driver to be installed option”. Then i tryied it this way, and installed “FTDIBUS.INF” and “FTDIPORT.INF” 3 times, since olimex is not telling which one to install 3 times, but this too is not helping.
Then i downloaded the drivers from FTDI directly, but these you can absolutely not install, so what am i to do? im helpless, i spend some bugs on this tool to go on developing with ARM.
I also noticed that there is no voltage output on the device.
So any help would really be apreciated.