Laser rangefinder code problems

Let me try to understand what’s working and what’s not. You have the laser rangefinder (LRF) connected to an Uno. The

LRF talks to the Uno via a TTL serial link (115k baud). The Uno talks to a Mega via a TTL serial link (9600 baud) ? The distance is sent via these serial links ? As an ASCII encoded data block, 8 times/sec. You can “print” the distance at the ?Uno and/or Mega? and it contains a correct value that will always, has always been 32m or less ?

The problem arises only when trying to write the data to the SD card ? Or when trying to get the distance from the Uno to the Mega, even w/o any SD card activity ongoing ? Or is the distance coming across the AUX serial link, directly from the LRF ?