I have a Livox Mid-360 connected to a SpartFun RTK I have a Livox Mid-360 connected to a SpartFun RTK ZED-F9P board. I have the PPS wire connected with a 1Hz PPS rate. The UART 1 is configured to 9600 Baud as that is the maximum rate the Livox Mid-360 will run. If I configure the UART 1 port to 1Hz rate and I configure the USB message rate to 1Hz everything remains in sync according to the Livox Viewer. If I change the USB message rate to 10Hz the Livox Mid-360 Livox Viewer on the PC will report intermittent sync loss roughly every 10 seconds or less.
How do I resolve this issue to allow a high frequency message rate to the PC on the USB connection while maintaining the 1Hz rate on the UART 1 to maintain sync with the Livox Mid-360? I have tried reducing messages and changing Baud rates as well as other suggestion from AI but nothing has helped. Is there an additional board to add that will allow the Livox to remain in sync with 10Hz message rate on the USB port? Is there a secret config that will support this?
Ok, but what did you actually set as message configurations?
Do you see any $GxTXT “txbuf,alloc” warnings in the output stream on USB?
The Livox only needs to see $GPRMC so all other should be disabled on UART1.
So you probably want to change the NMEA settings to report only GPS Talker ($GP) and a rate of 10 for RMC when the measurements/navigation is at 10 Hz so as decimate the output there to 1 Hz. However the decimation does not guarantee alignment with top-of-second, ie xxx.00 time stamp.
Hi Clive, Thanks for the info, I have cut all the unnecessary messages to only output $GPMRC. I do not see any txBuf,alloc warnings on the USB stream. I think the issue is that “decimation does not guarantee alignment with top-of-second, ie xxx.00 time stamp”. How do I overcome this to get better alignment? Is there an alternative setup option or additional hardware that would help?