LM3886 Amplifier Board

FartingMonkey92:
How much space are you going to save by redesigning this PCB?

Because you still have to locate a hefty transformer, rectifiers

and smoothing capacitors in your enclosure, plus panel connectors…

And you’ll still need a rather large heatsink to go with it, no point

skimping on that and using a smaller one after taking your time to

design the PCB and to stuff them…

Hopefully a few square inches. Not to mention its helping me learn eagle, but thats besides the point. And yes, I will still need caps and a big transformer, but those can be case mounted, they dont need to be mounted on the board :)

bigglez:

SpikedCola:
Added a new version, this time with a GND pour! Its a teeny bit oversized (the image) but I hope you guys dont mind - its hard to read if I go much smaller

Okay, much much better! Still have some

things to work on, though.

The single most agregous issue is that you have

inputs and outputs very close together. Doing so

runs a strong risk of feedback and oscillation.

Take a second look at the trace/tracks under C1.

The power traces are still way way way too thin.

Did you follow my instructions to bump up the

trace/track width?

You may keep the thin traces for some signals

around the IC, but the power, ground, and

output have to be at the very least 250mils.

I think there’s a serious error on the PCB in

the link, perhaps I’m missing something:

Isn’t C11 and C12 connected backwards?

Theyre both non-polarized as far as I can tell.

As for upping the size of the power traces, would I be better off doing a pour for them aswell? It seems that if I up the traces I have to manually route them, there must be an easier way :wink: