# Load Cell Output

**URL:** <https://community.sparkfun.com/t/load-cell-output/63776>\
**Category:** Force & Weight\
**Created:** [March 5, 2025, 2:55am UTC](https://community.sparkfun.com/t/load-cell-output/63776 "2025-03-05T02:55:39Z")\
**Posts on this page:** 4\
**Page:** 1

<div class="post-metadata">

**Author:** ![FlyingForts](https://avatars.discourse-cdn.com/v4/letter/f/65b543/32.png) [@FlyingForts](https://community.sparkfun.com/u/FlyingForts)\
**Post date:** [March 5, 2025, 2:55am UTC](https://community.sparkfun.com/t/load-cell-output/63776/1 "2025-03-05T02:55:39Z")

</div>

I’m a high school technology / engineering teacher looking for help on a classroom project. I’m hoping people with more electronics knowledge can help guide me in the correct direction.

I’m looking to use an S-style load cell for a homemade material strength tester. I would like to graph the output using Vernier’s Graphical Analysis Pro software. The software requires a 0-5V or 0-10V input signal.

My plan was to use an Arduino minima with a sparkfun load cell amplifier board. I would use the DAC on the minima to output the desired voltage to the vernier software. We do not need highly accurate measurements.

Does this sound reasonable? I have seen some load cell amplifier circuits online that output the desired voltage range but I have had back luck with imported boards in the past. I would like this system to be reliable or classroom use.

---

<div class="post-metadata">

**Author:** ![dilshana](https://avatars.discourse-cdn.com/v4/letter/d/f4b2a3/32.png) [@dilshana](https://community.sparkfun.com/u/dilshana)\
**Post date:** [March 5, 2025, 7:08am UTC](https://community.sparkfun.com/t/load-cell-output/63776/2 "2025-03-05T07:08:11Z")

</div>

Most S-type load cells output a very small signal in the millivolt range.  
You need a very precise amplifier. The DAC of the Arduino Minima only outputs 0-3.3V, not 0-5V. So, you have to scale it to 0-5V or 0-10V using an OP-AMP. I think it will be simpler if you use a Load cell, an HX711/ADS1232, an Arduino+External DAC and then connect the DAC output to the Vernier. Here are some more suggestion related to interfacing S-type load cells with the Arduino. [S Type Load Cell with Arduino and HX711 - Sensors - Arduino Forum](https://forum.arduino.cc/t/s-type-load-cell-with-arduino-and-hx711/1346043)

---

<div class="post-metadata">

**Author:** ![brow](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/brow/32/6116_2.png) [@brow](https://community.sparkfun.com/u/brow)\
**Post date:** [March 5, 2025, 2:46pm UTC](https://community.sparkfun.com/t/load-cell-output/63776/3 "2025-03-05T14:46:29Z")

</div>

Do you want a project or a solution? In the instrumentation biz, that’s called a _transmitter_. An industrial controller will do this effortlessly. They’re often in a DIN rail mount package for use in automation cabinets. Below are some reputable ones but I’m sure some cheaper ones are out there for the finding.

> **[1203 Weight Transmitter – Rinstrum](https://www.rinstrum.com/product/1203-weight-transmitter/)**

> **[SCT-30 Signal Conditioning Transmitter](https://www.ricelake.com/products/sct-30-signal-conditioning-transmitter/)**
>
> Rice Lake's compact SCT-30 signal conditioning transmitter delivers equivalent signal-conditioning function for PLC systems that require weight data from a scale, without the cost or bulk of a full-size weight indicator/controller.

Edit: They’re also called conditioners or just amplifiers.  
Some load cells have an amplifier built in using a device like this:

> **[ICA H & S](https://www.mantracourt.com/products/analog-output-signal-conditioners/miniature-strain-gauge-amplifier)**
>
> Miniature Strain Gauge Amplifier, Converts Load Cell to 4-20 mA & 0-10 V. The ICA amplifier small size for fitting inside sensors or in line with load cell.

Here’s some S beams with amplifiers:

> **[S-Beam - DC Output (V/MA) Load Cells | Buy Force Sensors at P3 America](https://p3america.com/load-cells-force-sensors/s-beam-load-cells/s-beam-analog-output/?srsltid=AfmBOoqwE2W5XVS-EXYqwM_W4hDjPzYP0-nrPQiHnwskQB0HnE_skCQl)**
>
> S-Beam load cells for tension and compression force measuring. 1 kN max. up to 10 kN max. Internal signal conditioner for 0 - 10V or 4 - 20mA output. Shop P3 today.

---

<div class="post-metadata">

**Author:** ![TS-Russell](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/ts-russell/32/6092_2.png) [@TS-Russell](https://community.sparkfun.com/u/TS-Russell)\
**Post date:** [March 5, 2025, 7:29pm UTC](https://community.sparkfun.com/t/load-cell-output/63776/4 "2025-03-05T19:29:35Z")

</div>

I’ll guess in this case they actually _do_ want a project (teacher & students) 🙂

Yes, your plan is reasonable…it’s fairly straightforward with the mentioned items, [just substitute the minima for the Redboard used in our guide](https://learn.sparkfun.com/tutorials/load-cell-amplifier-hx711-breakout-hookup-guide#hardware-hookup-)