Low side driver to control a seat blower motor

Im working on a car seat that has a cool function. The blower blower motor has a logic board in it. It is supplied with 12 volts and a ground. The ground side is controlled by the logic board via a pwm ground signal. Can anyone recommened a low side drive that would work?

Can you share a photo of what you’re describing?

Do you know the amperage of the blower motor?

any suggestions based on the wiring diagram?

I had a hard time reading it, but here’s my take given my understanding…For an OEM seat blower with logic board, & PWM ground control, you have two practical paths:

DIY Build

This is likely your cleanest/fastest solution:

  • MOSFET: IRLZ44N or IRFB4110PbF (this is just a guess, pick one sized ~2x the max current draw of the motor)

  • Gate Driver: TC4427 or UCC27517

  • Freewheeling Diode: MBR1045 Schottky

  • Perfboard + connectors:

  • Heat sink: Adding a small aluminum piece if the MOSFET doesn’t come with one might be a good idea to keep things cool

Wire it as: Motor Ground → Drain → Source → Chassis Ground, with the gate driven by your PWM source. The 12V feed stays constant.

Or, you could try to adapt a Pre-Made Module

If you want something closer to plug-and-play, look for:

  • “PWM solenoid driver” or “PWM valve controller” modules on Amazon/AliExpress — these are more likely to be true low-side switches

  • Infineon HITFET evaluation boards — automotive-qualified low-side smart switches, but you’ll need to source through distributors (DigiKey.com & Mouser.com are both excellent choices)

The main consideration will be the in-rush/max amp draw for the motor, which you will need to measure to determine and then pick a path above