Hi, I’m building a BMX race-timing system using the SparkFun Simultaneous RFID Reader — M7E Hecto, and I have a question about cable choice for the external antenna run.
Setup:
M7E Hecto with the RF resistor reflowed to the u.FL position (per the “Using an External Antenna” guide)
u.FL → RP-SMA pigtail (short, ~15cm) from the board
~10m cable run from the pigtail to a SparkFun UHF RFID Antenna (RP-TNC female pigtail on the antenna, 30cm)
Reader set to max power (27dBm / 500mW) via software
I’m deciding between RG-58 and LMR-240 for the 10m run. By my calculation at 915MHz:
RG-58: ~0.52dB/m → ~5.2dB over 10m
LMR-240: ~0.24dB/m → ~2.4dB over 10m
Combined with connector crossings (~0.5dB total for u.FL/RP-SMA/RP-TNC junctions), that’s roughly 5.9dB total loss with RG-58 (~129mW reaching the antenna) vs. 3.1dB with LMR-240 (~245mW reaching the antenna).
Questions:
Does SparkFun have an official recommendation for cable type on a 10m external-antenna run with this reader, or is LMR-240 a reasonable minimum?
For a BMX finish-line use case (want a controlled/short read range, not maximum range — to avoid false reads before the line), is there a preferred power level at the antenna, or is tuning purely done via the reader’s software power setting?
Thanks in advance — happy to share more setup details if useful.
Update on the cable question — I’m now leaning toward shortening the antenna run to 5m instead of 10m so I can stick with RG-58 rather than switching cable types.
Recalculating: at ~0.52dB/m, that’s ~2.6dB over 5m, plus the same ~0.5dB from the u.FL/RP-SMA/RP-TNC junctions ≈ 3.1dB total — which lands almost exactly where LMR-240 was at 10m (~245mW reaching the antenna at 27dBm).
If 5m is workable for my track layout, this seems like a reasonable way to keep the simpler/cheaper cable without giving up power budget. Does that check out, or is there a reason to prefer LMR-240 regardless of length (return loss, shielding, something else RG-58 handles worse)?
Second question, separate topic: what’s the recommended way to manage heat on the M7E Hecto’s ground plane/heatsink area during sustained operation at 27dBm? I’m considering a 30x30cm heatsink with a 5V USB fan, but I need to figure out the right way to physically secure it to the board — thermal adhesive/pad directly on the ground plane, standoffs through the mounting holes, or something else recommended by SparkFun/ThingMagic? Also open to hearing if a heatsink that size is overkill (or insufficient) for continuous high-power transmission in an enclosed case.
Thanks again — this has been really helpful for planning the finish-line hardware.
I think your second post is on the right ‘track’ (ha)…LMR is great but very pricey; the dB attenuation/signal loss difference likely won’t matter too much in-practice (as you’ll need to tune the read power anyhow, which in theory will compensate for such losses with higher read power). I’m guessing they’ll perform similarly when in-use
I’d say if there is basically any potential for moving/relocating the finish line RG would be better…the benefits of LMR probably won’t outweigh the cost + reduced flexibility
The main recommendation I have though is to look into a linear or polarized antenna to help with keeping the beam narrow/discrete for the finish line
Thanks for the great insight! The point about RG vs. LMR cables is spot on for my use case. Since this is a portable ‘appliance’ for BMX tracks, the flexibility and cost-effectiveness of RG-58 are much more valuable than the low attenuation of a rigid LMR-400. I can definitely compensate for the signal loss by tuning the M7E Hecto (which outputs up to 27 dBm), especially since I’m already adding active cooling (heatsink + fan) to handle the extra heat.
Regarding polarization, you’ve touched on a classic trade-off. While a linear antenna provides that ‘surgical’ narrow beam, BMX racing presents a high risk of Capture Effect. Riders are constantly jumping and changing their posture; if a tag isn’t perfectly aligned with a linear beam, the reader might miss it entirely. For the final version, I’m leaning towards a circular polarization mat (like the UA-6000) or a circular pencil-beam antenna (like the Advantenna-p33) to ensure I catch the tags regardless of their orientation.
For the current Laboratory Phase, I’ll be using the SparkFun UHF RFID Antenna (6dBi, RP-TNC). This is perfect for debugging the core logic—syncing the RFID trigger with our 240fps global shutter camera and the gate sensor—ensuring we can accurately cover the full 5.8-meter width of the finish line (standard for 8 lanes).
This is a serious, long-term project, so you’ll probably see me around this forum for a long time , especially when I get to the phase of integrating the professional-grade antennas and mats. Thanks again for helping me refine the hardware stack!