I’m using a LIDAR-Lite v4 LED and have a question about a measurement issue.
When rotating the sensor around the pitch axis, there is almost no distance error when it is facing upward, but when it is facing downward, the measurement error exceeds 10 cm.
I have already checked and ruled out housing/protective window/bracket internal reflection, target angle/reflectivity, cable tension, and PCB bending as possible causes.
Could this be related to DC bias correction, signal/reference overflow, high-accuracy averaging delay, or a detector/receiver alignment defect that only appears when measuring downward?
Please also let me know whether this symptom could indicate a defective unit and whether it would qualify for replacement.
The power was supplied to the laptop using a C-type port, and I ran it using the example code provided by your company.
The pins I’m using are 1, 2, 3, and 4, and the standard way to use power on pin 1 with the I2C protocol is 5V. However, in my case, when the lidar faced downwards, there was a 10cm error at 5V, which was resolved by switching to 3.3V.
What I’m asking is, will there be any lifespan issues if I continue to use 3.3V?
Sure - from the guide I linked above: “The I2C bus operates internally at 3.3 Vdc. Internal 13 kiloohm
pull-up resistors ensure this functionality and allow for a simple
connection to the I2C host”
Where in the link you provided does it say, “The I2C bus operates internally at 3.3 Vdc. Internal 13 kiloohm pull-up resistors ensure this functionality and allow for a simple connection to the I2C host”? On the contrary, there is content that allows us to infer that there are no internal registers, as shown in the following picture.
The main issue would be attempting to power a 3v device at 5v…this cooks things. Trying to power something a 5v device with 3v will usually result in it either turning on or not
The main thing to look for is to ensure the i2c/IO lines are 3.3v