PaulZC
April 7, 2025, 7:29am
4
Hi Clancey (@tyrian869 ),
Great detective work! I’m really glad you were able to fix this and get the NI LED to light up. Apologies for the hassle. Automated Optical Inspection must have missed that.
I’ll add a link to your other post below, just to close the circle.
Best wishes,
Paul
Okay I’m getting onboard with this sparkfun,
My setup is sparkfun SARA-R510M8S Gnss + LTE micromod function, a sparkfun ESP32 processor, Hologram sim, LTE wide band flec antenna 600mhz-6000mhz
My issue is that when using the example code #2 I never get a blue light as mentioned in sparkfuns guide, I can press any key and I get the following
All X’s are populated, just renamed for security reasons.
SARA-R5 connected!
Manufacturer ID: u-blox
Model ID: SARA-R510M8S
Firmware Version: 03.30
Product Serial No.: XXXXXXXXXXXXXX
IMEI: XXXXXXXXXXXXX
IMSI: XXXXXXXXXXXXX
SIM CCID: XXXXXXXXXXXXXXXX
Subscriber No.:
Capabilities: +CGSM
SIM state reports requested…
That’s all I get.
More so If I try and use the M-Center to try and connect I get the following (Not responding) and the only time I do get any information is just after I connect the USB and connect only for the first connect will it give me any information. The firmware appears to be the latest so IDK what to think, It can’…