# Module charger for LiPo Battery

**URL:** <https://community.sparkfun.com/t/module-charger-for-lipo-battery/35355>\
**Category:** Projects\
**Created:** [March 11, 2018, 6:55pm UTC](https://community.sparkfun.com/t/module-charger-for-lipo-battery/35355 "2018-03-11T18:55:06Z")\
**Posts on this page:** 1\
**Page:** 1

<div class="post-metadata">

**Author:** ![akinet](https://avatars.discourse-cdn.com/v4/letter/a/a6a055/32.png) [@akinet](https://community.sparkfun.com/u/akinet)\
**Post date:** [March 11, 2018, 6:55pm UTC](https://community.sparkfun.com/t/module-charger-for-lipo-battery/35355/1 "2018-03-11T18:55:06Z")

</div>

Hi.

I don’t know if this is the right forum to post this question. So, if I’m wrong, excuse me.

I am trying to repair a tablet that is fully operational but the usb port is broken, so I cannot charge its battery. I have ruled out the possibility of replacing the usb port because of the complexity of welding such small tracks. So I am thinking in charge the battery directly, because it’s easy to connect a charger to the battery cables. The battery inside is a LiPo battery 6500mAh. I have found the specifications on this link: [https://www.aliexpress.com/item/2613014 … 52639.html](https://www.aliexpress.com/item/26130147-3-7V-6500MAH-lithium-polymer-battery-backup-power-supply-3-7V-Tablet-battery-Rechargeable-batteries/32835152639.html)

**Specifications** :

1,Nominal voltage:3.7V;

2,Standard charge and discharge at 1C

**Feature** :

3.7v lithium battery pack for psp battery

Charge current: standard 0.2 C5A and maximum 1C5A

Charge cut-off voltage: 4.20 0.03V

Standard discharge current: 0.2C5A

Maximum discharge current: 2.0C5A

Discharge cut-off voltage: 2.75V

So I want to know, what specifications should have a charger module to connect directly to the battery? I am worried about risk of overheating and explosion.

I have seen several charger modules but i am not sure if they can charge this battery without problems.

Module 1

=========

Features:

Battery over discharge protection voltage: 2.5V

Battery over-current protection current: 3A

Support charging&discharging at the same time

Parameter:

The input voltage: 5V

Maximum charging current: 1000 mA

Charge cut-off voltage: 4.2 V + / - 1%

Module 2

=========

Description:

1.Module type: Lipo Battery Charging Board

2.Charge mode: Linear charging

3.Charge Current: 1A

4.Charge precision: 1.5 %

5.Input voltage: 4.5V ~ 5.5V

6.Full charged voltage: 4.2 V

7.Led indicator: Red is charging, Blue is full charged

Module 3

=========

Features:

2 in 1 charge and Discharger(boost) modules

Charge voltage : DC 4.6V-8V(Recommend DC 5V)

Charging current : 0-1A

Full charge voltage : 4.2V±2%.

Led indicator : “OK” LED is fully charged OR battery failure status indicator;

“CR” LED is charge status indicator

Discharge current : 0-2A;

Discharge quiescent current : 450uA

Discharge conversion efficiency : 78%-90%

Output current : 0-1.2A（5V）;

This module without lithium battery over-discharge protection.

* * *

Can this charge modules work for that battery? Should I look for different charger modules?

Regards.

akinet