# nRF52810 & Raspi - Failed to erase reg: 0x4001e50c val: 0x00000001

**URL:** <https://community.sparkfun.com/t/nrf52810-raspi-failed-to-erase-reg-0x4001e50c-val-0x00000001/35720>\
**Category:** MicroMod\
**Tags:** arm-lpc\
**Created:** [July 29, 2018, 11:17am UTC](https://community.sparkfun.com/t/nrf52810-raspi-failed-to-erase-reg-0x4001e50c-val-0x00000001/35720 "2018-07-29T11:17:06Z")\
**Posts on this page:** 1\
**Page:** 1

<div class="post-metadata">

**Author:** ![kaefert](https://avatars.discourse-cdn.com/v4/letter/k/8797f3/32.png) [@kaefert](https://community.sparkfun.com/u/kaefert)\
**Post date:** [July 29, 2018, 11:17am UTC](https://community.sparkfun.com/t/nrf52810-raspi-failed-to-erase-reg-0x4001e50c-val-0x00000001/35720/1 "2018-07-29T11:17:06Z")

</div>

I would like to flash an nRF52810 board by using OpenOCD running on an Raspberry Pi 1 B Rev2.

I built and installed OpenOCD on my Pi like so:

```auto
git clone https://git.code.sf.net/p/openocd/code openocd-code
cd openocd-code
./bootstrap
./configure --enable-sysfsgpio --enable-bcm2835gpio
make
sudo make install

```

Between checking out and building I’ve modified nrf5.c to include this line:

NRF5\_DEVICE\_DEF(0x0139, “52832”, “QFAA”, “E0”, 512),

I’ve connected these nRF52810 Pins to those Pi Pins:

```auto
SWDIO <-> GPIO24
SWDCLK <-> GPIO25
P021=RST <-> GPIO18

```

I’m using this openocd.cfg file:

```auto
source [find interface/raspberrypi-native.cfg]
bcm2835gpio_speed_coeffs 113714 28
bcm2835gpio_swd_nums 25 24
bcm2835gpio_srst_num 18
reset_config srst_only srst_push_pull
transport select swd
set WORKAREASIZE 0
set CHIPNAME nrf52810
source [find target/nrf51.cfg]
reset_config srst_only srst_nogate
adapter_nsrst_delay 100
adapter_nsrst_assert_width 100
init
targets
halt
nrf5 mass_erase
flash write_image feather52_bootloader_v050_s132_v201.hex 0
reset halt
targets
verify_image feather52_bootloader_v050_s132_v201.hex 0
reset run
targets
exit

```

And I’m getting this output:

```auto
Info : BCM2835 GPIO JTAG/SWD bitbang driver
Info : JTAG and SWD modes enabled
Info : clock speed 1006 kHz
Info : SWD DPIDR 0x01a93070
Info : SWD DPIDR 0x2ba01477
Info : nrf52810.cpu: hardware has 6 breakpoints, 4 watchpoints
Error: nrf52810.cpu -- clearing lockup after double fault
Polling target nrf52810.cpu failed, trying to reexamine
Info : nrf52810.cpu: hardware has 6 breakpoints, 4 watchpoints
Info : Listening on port 3333 for gdb connections
    TargetName Type Endian TapName State       
-- ------------------ ---------- ------ ------------------ ------------
 0* nrf52810.cpu cortex_m little nrf52810.cpu halted
Info : nRF52810-QFAA(build code: Bx0) 192kB Flash
Error: Failed to erase reg: 0x4001e50c val: 0x00000001
Error: Failed to erase the chip

```

Trying to flash without the mass erase gives this output:

```auto
Info : nRF52810-QFAA(build code: Bx0) 192kB Flash
Info : Padding image section 0 at 0x00000964 with 1692 bytes
Warn : not enough working area available(requested 32)
Warn : no working area available, falling back to slow memory writes
Warn : no flash bank found for address 0x00074000
Warn : not enough working area available(requested 36)
Running slow fallback erase check - add working memory
Warn : not enough working area available(requested 32)
Warn : no working area available, falling back to slow memory writes
wrote 112336 bytes from file feather52_bootloader_v050_s132_v201.hex in 11.031472s (9.945 KiB/s)
target halted due to debug-request, current mode: Handler HardFault
xPSR: 0x01000003 pc: 0xfffffffe msp: 0xffffffd8
    TargetName Type Endian TapName State       
-- ------------------ ---------- ------ ------------------ ------------
 0* nrf52810.cpu cortex_m little nrf52810.cpu halted
Warn : not enough working area available(requested 52)
Warn : not enough working area available(requested 52)
Warn : not enough working area available(requested 52)
Error: checksum mismatch - attempting binary compare
diff 0 address 0x00074000. Was 0x00 instead of 0x80
diff 1 address 0x00074001. Was 0x00 instead of 0x7f
...
diff 127 address 0x000740c5. Was 0x00 instead of 0x94
More than 128 errors, the rest are not printed.

```

Can you help me?

On the [[nordicsemi forum](https://devzone.nordicsemi.com/f/nordic-q-a/36813/openocd-nrf52810-can-t-erase-or-flash---unknown-device-hwid-0x00000142) an engineer told me OpenOCD only supports the nRF52832 chip and not the nRF52810 and I need to use an SEGGER debugger instead. But I figured those two chips are almost the same and adding support shouldn’t involve too much of a hassle. Can you tell me what needs to be done? On the same forum there is a post that reads like other people have already figured it out: [https://devzone.nordicsemi.com/f/nordic … spberry-pi](https://devzone.nordicsemi.com/f/nordic-q-a/33140/programming-nrf52810-with-openocd-and-raspberry-pi)]([OpenOCD nRF52810: Can't erase or flash - Unknown device HWID 0x00000142 - Nordic Q&A - Nordic DevZone - Nordic DevZone](https://devzone.nordicsemi.com/f/nordic-q-a/36813/openocd-nrf52810-can-t-erase-or-flash---unknown-device-hwid-0x00000142))