OLED for DEV-22925

Is there an OLED that fits on the esp32 pocket development board, SKU: DEV-22925, like the image below?

There are 2 potential options:

SparkFun Micro OLED Breakout (Qwiic) - SparkFun Electronics which is sized like so

SparkFun Micro OLED Breakout (with Headers) - SparkFun Electronics which doesn’t have mounting screw holes but you may prefer it

The first one also has 2 qwiic ports which make things a bit easier