http://www.flickr.com/photos/wannabefren/3860158811/
http://www.flickr.com/photos/wannabefren/3860158817/
http://www.flickr.com/photos/wannabefren/3860173321/
Above is the 3 pic i have uploaded. It’s the board and Jtag device that i am working on to detect the board.
This Jtag device is the USB_Jtag version that i am working on, not the olimex or amotec type device. Being trying hard to solve the problem, hoping anyone out there could advice. Since the FTDI chip i am using is a dual channel, i have edited the CDM FTDI to manually installed one channel and use the libusb-win32 to install another channel. Vid and Pid are both 0x0403 and 0x6010.
Am i right doing the above steps? OOCD link type, is it advised?
This is the ftdibus.inf i have added in to manually install
[FtdiHw]
%USB\VID_0403&PID_6010&MI_00.DeviceDesc%=FtdiBus.NT,USB\VID_0403&PID_6010&MI_00
%USB\VID_0403&PID_6010&MI_01.DeviceDesc%=FtdiBus.NT,USB\VID_0403&PID_6010&MI_01
[FtdiHw.NTamd64]
%USB\VID_0403&PID_6010&MI_00.DeviceDesc%=FtdiBus.NTamd64,USB\VID_0403&PID_6010&MI_00
%USB\VID_0403&PID_6010&MI_01.DeviceDesc%=FtdiBus.NTamd64,USB\VID_0403&PID_6010&MI_01
[Strings]
Ftdi=“FTDI”
DESC=“CDM Driver Package”
DriversDisk=“FTDI USB Drivers Disk”
USB\VID_0403&PID_6010&MI_00.DeviceDesc=“OOCDLINK USB Serial Converter A”
USB\VID_0403&PID_6010&MI_01.DeviceDesc=“OOCDLINK USB Serial Converter B”
SvcDesc=“USB Serial Converter Driver”
ClassName=“USB”
ftdiport.inf
[FtdiHw]
%VID_0403&PID_6010.DeviceDesc%=FtdiPort2232.NT,FTDIBUS\COMPORT&VID_0403&PID_6010
[FtdiHw.NTamd64]
%VID_0403&PID_6010.DeviceDesc%=FtdiPort2232.NTamd64,FTDIBUS\COMPORT&VID_0403&PID_6010
[Strings]
FTDI=“FTDI”
DESC=“CDM Driver Package”
DriversDisk=“FTDI USB Drivers Disk”
PortsClassName = “Ports (COM & LPT)”
VID_0403&PID_6010.DeviceDesc=“USB Serial Port”
SvcDesc=“USB Serial Port Driver”
SerEnum.SvcDesc=“Serenum Filter Driver”
for libusb-win32.inf
[Devices]
“Channel B”=LIBUSB_DEV, USB\VID_0403&PID_6010&MI_01
[Devices.NT]
“Channel B”=LIBUSB_DEV, USB\VID_0403&PID_6010&MI_01
I have added on channel B of the Jtag to libusb and Channel A to FTDI CDM. Still i cant get the device found. Trying to work on window platform instead of Linux environment.
I have seen alot of forum using cygwin and i am using yargato GNU arm, will it work out to be fine?
Sorry to trouble you all, and thx for advice too from chopin and dougm84