# OpenOCD JTAG interrogation failed: all ones

**URL:** <https://community.sparkfun.com/t/openocd-jtag-interrogation-failed-all-ones/19357>\
**Category:** MicroMod\
**Tags:** arm-lpc\
**Created:** [February 9, 2011, 12:13am UTC](https://community.sparkfun.com/t/openocd-jtag-interrogation-failed-all-ones/19357 "2011-02-09T00:13:17Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![cgili](https://avatars.discourse-cdn.com/v4/letter/c/45deac/32.png) [@cgili](https://community.sparkfun.com/u/cgili)\
**Post date:** [February 9, 2011, 12:13am UTC](https://community.sparkfun.com/t/openocd-jtag-interrogation-failed-all-ones/19357/1 "2011-02-09T00:13:17Z")

</div>

Spent the better part of the day on Google, looking for a resolution, but most hits resolve to questions about the hardware being bad. I hope the problem is with my config file and not with the hardware. The board in question functions otherwise and I can program it serially, so I don’t think it’s toasted. Anyone have any suggestions as to what to try next? Time to break out the o-scope and start watching the JTAG lines?

First, my OpenOCD setup:

-Windows 7 with MINGW

-Amontec JTAGkey-Tiny v1.0

-Amontec JTAGkey drivers v2.6.0.0

-LibUSB Filter v1.2.2.0

-OpenOCD 0.4.4 (2010-02-22-19:05) from Freddie Chopin’s msi installer

Now, hardware. I have two Keil eval boards:

1. MCB1700 with a LPC1768

2. MCB2300 with a LPC2387

Board #1 works fine with the file included with openocd (./board/keil\_mcb1700.cfg) . The problem is that board #2 produces the following output:

> $ openocd -f /s/embedded/lpc23xx/doc/lpc2387\_jtag.cfg
> 
> Open On-Chip Debugger 0.4.0 (2010-02-22-19:05)
> 
> Licensed under GNU GPL v2
> 
> For bug reports, read
> 
> [http://openocd.berlios.de/doc/doxygen/bugs.html](http://openocd.berlios.de/doc/doxygen/bugs.html)
> 
> debug\_level: 2
> 
> 200 kHz
> 
> trst\_and\_srst srst\_pulls\_trst srst\_gates\_jtag trst\_push\_pull srst\_
> 
> jtag\_nsrst\_delay: 100
> 
> jtag\_ntrst\_delay: 100
> 
> Info : clock speed 200 kHz
> 
> Error: JTAG scan chain interrogation failed: all ones
> 
> Error: Check JTAG interface, timings, target power, etc.
> 
> Error: JTAG scan chain interrogation failed: all ones
> 
> Error: Check JTAG interface, timings, target power, etc.
> 
> Command handler execution failed
> 
> Warn : jtag initialization failed; try ‘jtag init’ again.

I didn’t see any included config files for the second board, so I snipped together the following from other examples:

```auto
# OpenOCD config file for LPC2387

# minimal debugging
debug_level 1

# daemon configuration
telnet_port 4444
gdb_port 3333
tcl_port 6666

# interface
interface ft2232
ft2232_device_desc "Amontec JTAGkey"
ft2232_layout jtagkey
ft2232_vid_pid 0x0403 0xcff8

# speed
jtag_khz 200

# reset configuration
reset_config trst_and_srst srst_pulls_trst
jtag_nsrst_delay 100
jtag_ntrst_delay 100

# create a tap
jtag newtap lpc2387 cpu -irlen 4 -ircapture 0x1 -irmask 0xf -expected-id 0x4f1f0f0f

# create a target
target create lpc2387.cpu arm7tdmi -endian little -chain-position lpc2387.cpu -variant arm7tdmi-s_r4
lpc2387.cpu configure -work-area-phys 0x40000000 -work-area-size 0x10000 -work-area-backup 0

# flash configuration
flash bank lpc2000 0x0 0x80000 0 0 lpc2387.cpu lpc2000_v2 4000 calc_checksum

```

---

<div class="post-metadata">

**Author:** ![cgili](https://avatars.discourse-cdn.com/v4/letter/c/45deac/32.png) [@cgili](https://community.sparkfun.com/u/cgili)\
**Post date:** [February 10, 2011, 3:52pm UTC](https://community.sparkfun.com/t/openocd-jtag-interrogation-failed-all-ones/19357/2 "2011-02-10T15:52:34Z")

</div>

Turns out it was my JTAG adapter. I’m using a 10-pin JTAG header, along with the Embedded Artists 20-to-10 pin adapter. This works just fine on the Keil MCP1700 (after changing the “reset\_config” option to “srst\_only”), but since I’m using a LPC2468 on my board, I apparently need TRST. I tried lots of different permutations for “reset\_config”, but then I added a discrete wire for TRST and it works.