OpenOCD with Olimex ARM-USB-OCD-H

I created sym links for libusb.* and libftdi.* . The ft2232 interface is available now.

Now I’ve to figure out how to get JTAG work -

 openocd -f interface/olimex-arm-usb-ocd-h.cfg  -f target/cs351x.cfg
Open On-Chip Debugger 0.6.1 (2013-05-03-18:41)
Licensed under GNU GPL v2
For bug reports, read
        http://openocd.sourceforge.net/doc/doxygen/bugs.html
Info : only one transport option; autoselect 'jtag'
dcc downloads are enabled
Info : max TCK change to: 30000 kHz
Error: An adapter speed is not selected in the init script. Insert a call to adapter_khz or jtag_rclk to proceed.
in procedure 'init'