# Power for capacitive touch sensor AT42QT1010

**URL:** <https://community.sparkfun.com/t/power-for-capacitive-touch-sensor-at42qt1010/62356>\
**Category:** Other\
**Created:** [December 17, 2024, 10:08pm UTC](https://community.sparkfun.com/t/power-for-capacitive-touch-sensor-at42qt1010/62356 "2024-12-17T22:08:08Z")\
**Posts on this page:** 5\
**Page:** 1

<div class="post-metadata">

**Author:** ![solitary](https://avatars.discourse-cdn.com/v4/letter/s/ec9cab/32.png) [@solitary](https://community.sparkfun.com/u/solitary)\
**Post date:** [December 17, 2024, 10:08pm UTC](https://community.sparkfun.com/t/power-for-capacitive-touch-sensor-at42qt1010/62356/1 "2024-12-17T22:08:08Z")

</div>

I have a question about the SparkFun Capacitive Touch Breakout - AT42QT1010…

Specifically:  
I was attempting to use battery power for this device and hooked up 3 AA batteries in series to yield 4.5V. Put the +pole into the VDD pin & the – pole into the GND. It seemed to work partially—when the sensor was touched, the LED came on and there was a voltage signal from the out pin—however, the voltage was much smaller than expected, less than 100uV. Also, the baseline seemed noisy.

When the same component was powered via an Arduino board after connecting the Arduino power via a USB to a computer, it also functioned, but the output signal voltage was +5V.

Finally, I am wondering if one could power the AT42QT1010 using the power output from a USB cable connected to a wall charger… or if there might be a current overload.

Thanks so much for any info.

---

<div class="post-metadata">

**Author:** ![TS-Russell](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/ts-russell/32/6092_2.png) [@TS-Russell](https://community.sparkfun.com/u/TS-Russell)\
**Post date:** [December 18, 2024, 12:10am UTC](https://community.sparkfun.com/t/power-for-capacitive-touch-sensor-at42qt1010/62356/2 "2024-12-18T00:10:08Z")

</div>

You could try 4 batteries instead? It sounds underpowered

Yes, USB from a wall charger should be fine…or even a portable battery pack

---

<div class="post-metadata">

**Author:** ![solitary](https://avatars.discourse-cdn.com/v4/letter/s/ec9cab/32.png) [@solitary](https://community.sparkfun.com/u/solitary)\
**Post date:** [December 18, 2024, 1:27am UTC](https://community.sparkfun.com/t/power-for-capacitive-touch-sensor-at42qt1010/62356/3 "2024-12-18T01:27:08Z")

</div>

Thank you. Let me try. I was worried that with the 4 batteries is would be 6V and be too much for the circuit…

---

<div class="post-metadata">

**Author:** ![TS-Russell](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/ts-russell/32/6092_2.png) [@TS-Russell](https://community.sparkfun.com/u/TS-Russell)\
**Post date:** [December 19, 2024, 10:16pm UTC](https://community.sparkfun.com/t/power-for-capacitive-touch-sensor-at42qt1010/62356/4 "2024-12-19T22:16:16Z")

</div>

Eh, the voltage regulator is rated for 5.5, the chip it good until 6v…I’d try USB first and see if it is normal. Then you can test the batteries; there’s likely enough headroom/voltage drop for it to be fine…if it burns it up I’ll send ya a new one 😉

---

<div class="post-metadata">

**Author:** ![solitary](https://avatars.discourse-cdn.com/v4/letter/s/ec9cab/32.png) [@solitary](https://community.sparkfun.com/u/solitary)\
**Post date:** [December 20, 2024, 1:29am UTC](https://community.sparkfun.com/t/power-for-capacitive-touch-sensor-at42qt1010/62356/5 "2024-12-20T01:29:12Z")

</div>

Thank you TS-Russel.

Using the batteries the LED comes on but the output signal is very small. USB to computer works perfectly. USB plugged into a wall charger sends it into an oscillatory mode giving repetitive 5V signals! …. So interesting that the batteries don’t really work; I’m guessing not enough current. But all good, I can use the computer output to the USB…

Susan