# power supply for EM-406

**URL:** <https://community.sparkfun.com/t/power-supply-for-em-406/1243>\
**Category:** Development Boards\
**Created:** [January 7, 2006, 10:04pm UTC](https://community.sparkfun.com/t/power-supply-for-em-406/1243 "2006-01-07T22:04:40Z")\
**Posts on this page:** 7\
**Page:** 1

<div class="post-metadata">

**Author:** ![NleahciM](https://avatars.discourse-cdn.com/v4/letter/n/dc4da7/32.png) [@NleahciM](https://community.sparkfun.com/u/NleahciM)\
**Post date:** [January 7, 2006, 10:04pm UTC](https://community.sparkfun.com/t/power-supply-for-em-406/1243/1 "2006-01-07T22:04:40Z")

</div>

Now to start my 3rd topic on this module… Hopefully my last, but that’s doubtful.

I am trying to figure out the power supply for this little bugger. The manual calls for 4.5-6.5VDC, but does not elaborate any more on power supply requirements. On my board I have a very noisy 6V supply. It has 18 motors connected to it that are constantly pulsing on and off. Is this suitable?

I thought about the possibility of running the 6V through something like a 5V LDO and then filtering the 5V signal. Would that be an improvement, or will the EM-406 module care about the noisy supply line?

Thanks!

---

<div class="post-metadata">

**Author:** ![sparky](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/sparky/32/6021_2.png) [@sparky](https://community.sparkfun.com/u/sparky)\
**Post date:** [January 23, 2006, 11:03pm UTC](https://community.sparkfun.com/t/power-supply-for-em-406/1243/2 "2006-01-23T23:03:46Z")

</div>

Hi,

My two cents : GPS receivers need as clean a power supply as you can give them. Motors flipping direction can put so really nasty power spikes on the power system. I’d recommend isolation the logic from the drive train if possible.

-Nathan

---

<div class="post-metadata">

**Author:** ![system](https://canada1.discourse-cdn.com/sparkfun/original/2X/d/d19eb507aca5e19aadba71e3743536c935c64e77.svg) [@system](https://community.sparkfun.com/u/system)\
**Post date:** [January 24, 2006, 8:46am UTC](https://community.sparkfun.com/t/power-supply-for-em-406/1243/3 "2006-01-24T08:46:44Z")

</div>

HI,

Can I ask how to collect the data from the EM-406, or just give power and the dta will automatically output. Can I connect it with RS232 or I need to convert it. Please advise

---

<div class="post-metadata">

**Author:** ![brianhomer](https://avatars.discourse-cdn.com/v4/letter/b/57b2e6/32.png) [@brianhomer](https://community.sparkfun.com/u/brianhomer)\
**Post date:** [January 24, 2006, 8:58am UTC](https://community.sparkfun.com/t/power-supply-for-em-406/1243/4 "2006-01-24T08:58:24Z")

</div>

Dear sparky,

I am starting use the recent ordered EM-406, However, I need some example to connect it and get the data. where can I get this from?

I assumed use the MAX232 IC to convert the TTL to RS232 level, am I correct. then I can use RS232 collect the data. any important points I ignored?

Please comment! thank you!

Brian ho

---

<div class="post-metadata">

**Author:** ![NleahciM](https://avatars.discourse-cdn.com/v4/letter/n/dc4da7/32.png) [@NleahciM](https://community.sparkfun.com/u/NleahciM)\
**Post date:** [January 24, 2006, 4:45pm UTC](https://community.sparkfun.com/t/power-supply-for-em-406/1243/5 "2006-01-24T16:45:41Z")

</div>

> sparky:  
> Hi,
> 
> My two cents : GPS receivers need as clean a power supply as you can give them. Motors flipping direction can put so really nasty power spikes on the power system. I’d recommend isolation the logic from the drive train if possible.
> 
> -Nathan

Hi Nathan - I ended up using a 1mh super low resistance inductor in series with the +6V line as well as two ultra low resistance caps, a 10uf tantalum and a .1uf ceramic, going from EM-406 supply to EM-406 ground. I got a message back from tech support at usglobalsat where they said:

“No problems are found if you utilized a 6V line within 100mV noise. If noise exceeds 100mV, it may affect EM406 performance. Adding a bypass capacitor and using 5V LDO on the 6V line are both feasible. An alternative to this, is adding a bead on the 6V line.”

so I think my solution should be more than adequate.

> Anonymous:  
> HI,
> 
> Can I ask how to collect the data from the EM-406, or just give power and the dta will automatically output. Can I connect it with RS232 or I need to convert it. Please advise

Give it power and it will start spitting out NMEA 0183 data over the uart. this is all outlined in the datasheet, which you have obviously not read.

> brianhomer:  
> Dear sparky,
> 
> I am starting use the recent ordered EM-406, However, I need some example to connect it and get the data. where can I get this from?
> 
> I assumed use the MAX232 IC to convert the TTL to RS232 level, am I correct. then I can use RS232 collect the data. any important points I ignored?
> 
> Please comment! thank you!
> 
> Brian ho

A max232 circuit is indeed all you need to connect the EM-406 to a RS-232 line.

---

<div class="post-metadata">

**Author:** ![brianhohk](https://avatars.discourse-cdn.com/v4/letter/b/edb3f5/32.png) [@brianhohk](https://community.sparkfun.com/u/brianhohk)\
**Post date:** [January 25, 2006, 2:10am UTC](https://community.sparkfun.com/t/power-supply-for-em-406/1243/6 "2006-01-25T02:10:12Z")

</div>

Understood and much appreciated!

---

<div class="post-metadata">

**Author:** ![mericas](https://avatars.discourse-cdn.com/v4/letter/m/8baadc/32.png) [@mericas](https://community.sparkfun.com/u/mericas)\
**Post date:** [January 25, 2006, 5:49pm UTC](https://community.sparkfun.com/t/power-supply-for-em-406/1243/7 "2006-01-25T17:49:33Z")

</div>

I was hoping I could power the GPS directly from a battery since all the other components on the board were 3.3V. I tried using 4 AA batteries and it worked, sort of. Not very reliable. I finally added a 5V LDO for the GPS and now it is very happy.

Now I want to redesign my board with a 5V LDO feeding the GPS and the 3.3V LDO (instead of both LDO’s running off the supply voltage). I was thinking about switching regulators but LDOs are so easy, and cheap.