# Questions the NIR AS7263

**URL:** <https://community.sparkfun.com/t/questions-the-nir-as7263/65833>\
**Category:** Sensors\
**Created:** [July 1, 2025, 4:27am UTC](https://community.sparkfun.com/t/questions-the-nir-as7263/65833 "2025-07-01T04:27:11Z")\
**Posts on this page:** 4\
**Page:** 1

<div class="post-metadata">

**Author:** ![Angie\_Rivera](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/angie_rivera/32/10217_2.png) [@Angie\_Rivera](https://community.sparkfun.com/u/Angie_Rivera)\
**Post date:** [July 1, 2025, 4:27am UTC](https://community.sparkfun.com/t/questions-the-nir-as7263/65833/1 "2025-07-01T04:27:11Z")

</div>

Hello,

I am using the NIR AS7263 sensor to determine the Brix value in mandarin juice, and I have a couple of questions.

Currently, I am using a white LED light in a closed enclosure, but I am not sure if this is the correct light, as I have noticed significant variations between the readings taken with this light and those taken with ambient light.

1. How should I configure the light to correctly measure reflectance and ensure that the sensor is reading accurately?
2. Is it necessary to use a specific type of light or calibrate the sensor in any way to obtain precise measurements?

Additionally, this sensor has a measurement range of 610 nm to 860 nm, but generally, NIR spectra start at 800 nm.

1. Could it be said that this sensor measures both visible and infrared light, given that its range includes wavelengths within the visible light spectrum (610-750 nm)?

Thank you for your help.

Best regards,

---

<div class="post-metadata">

**Author:** ![TS-Russell](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/ts-russell/32/6092_2.png) [@TS-Russell](https://community.sparkfun.com/u/TS-Russell)\
**Post date:** [July 1, 2025, 6:30am UTC](https://community.sparkfun.com/t/questions-the-nir-as7263/65833/2 "2025-07-01T06:30:05Z")

</div>

> [@Angie\_Rivera](#):
>
> am using a white LED light in a closed enclosure, but I am not sure if this is the correct light, as I have noticed significan

1. Calibrate against your light source in the enclosed area vs the same area un-lit/dark

2. Yes, you’ll want a light source with a small frequency output range…some white LEDs will fit the bill, but you’ll want to ensure its specs are desirable. You can also test with different ones to watch how the data shifts

3. Yep…the only way to mitigate this is calibrating

---

<div class="post-metadata">

**Author:** ![jremington](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/jremington/32/6595_2.png) [@jremington](https://community.sparkfun.com/u/jremington)\
**Post date:** [July 5, 2025, 4:07am UTC](https://community.sparkfun.com/t/questions-the-nir-as7263/65833/3 "2025-07-05T04:07:55Z")

</div>

You might discuss the approach with @Manuel_Crisanta, who appears to have the exact same project.

> [@AS7263 Measurements / NIR Light / Consultations](https://community.sparkfun.com/t/as7263-measurements-nir-light-consultations/65835):
>
> Hello, I am using the NIR sensor AS7263 to determine the Brix degree in mandarin juice, and I have a couple of questions.Currently, I am using a white LED light in a closed environment, but I am not sure if this is the right light, as I have noticed significant variations between the measurements taken with this light and those made with ambient light. How should I set up the light to correctly measure reflectance and ensure that the sensor is reading correctly? Is it necessary to use a specific type of light or calibrate the sensor in any way to obtain accurate measurements?Additionally, this sensor has a measurement range of 610 nm to 860 nm, but generally NIR spectra start from 800 nm. Can it be said that this sensor measures both visible and infrared light, given that its range includes wavelengths within visible light (610-750 nm)? Thank you for your help. Regards,

---

<div class="post-metadata">

**Author:** ![Angie\_Rivera](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/angie_rivera/32/10217_2.png) [@Angie\_Rivera](https://community.sparkfun.com/u/Angie_Rivera)\
**Post date:** [August 2, 2025, 6:32pm UTC](https://community.sparkfun.com/t/questions-the-nir-as7263/65833/4 "2025-08-02T18:32:26Z")

</div>

jajajajaja de hecho somos compañeros