# QWIIC GPS-RTK2 CONNECT TO GROVE PORT ON M5STACK

**URL:** <https://community.sparkfun.com/t/qwiic-gps-rtk2-connect-to-grove-port-on-m5stack/37896>\
**Category:** Qwiic System\
**Tags:** qwiic\
**Created:** [October 5, 2019, 10:57am UTC](https://community.sparkfun.com/t/qwiic-gps-rtk2-connect-to-grove-port-on-m5stack/37896 "2019-10-05T10:57:38Z")\
**Posts on this page:** 4\
**Page:** 1

<div class="post-metadata">

**Author:** ![udangpindang](https://avatars.discourse-cdn.com/v4/letter/u/dbc845/32.png) [@udangpindang](https://community.sparkfun.com/u/udangpindang)\
**Post date:** [October 5, 2019, 10:57am UTC](https://community.sparkfun.com/t/qwiic-gps-rtk2-connect-to-grove-port-on-m5stack/37896/1 "2019-10-05T10:57:38Z")

</div>

Hello everyone!

I’m really newbie on this field as this is my first project and the qwiic really helpful to build it.

I have several question about connecting the gps to m5stack via it’s grove port.

a. The M5stack grove port is 5V instead 3V3. Does the Qwiic bus on GPS-RTK2 has 3.3V regulator?

b. Is it okay to connect the qwiic 3V3 pin to 3V3 on M5stack side Header? (it is an ESP32 and i think the logic level is the same with GPS of 3.3v)

c. Or i need some i2c logic level converter?

I’ve been looking the explanation on some cases of another 3V3 module, but i think it is better to make sure first in sparkfun forum.

Thank you for the reply!

 ![M5STACK.JPG](https://canada1.discourse-cdn.com/sparkfun/original/3X/a/4/a414bd6f5601be4cce78b6380735e89917561128.jpeg)

 ![M5STACK4.JPG](https://canada1.discourse-cdn.com/sparkfun/original/3X/3/0/30d3f4259487ca2db50e5867cbaf19e7dc095dee.jpeg)

 ![M5STACK3.JPG](https://canada1.discourse-cdn.com/sparkfun/original/3X/f/6/f640236b61b37e3917d76685aefbe4578cc631c9.jpeg)

---

<div class="post-metadata">

**Author:** ![El\_Duderino](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/el_duderino/32/6367_2.png) [@El\_Duderino](https://community.sparkfun.com/u/El_Duderino)\
**Post date:** [October 11, 2019, 5:39pm UTC](https://community.sparkfun.com/t/qwiic-gps-rtk2-connect-to-grove-port-on-m5stack/37896/2 "2019-10-11T17:39:49Z")

</div>

Hi udangpindang,

The Qwiic connector on the GPS-RTK2 does not have a regulator on it as it taps into the 3.3V rail after the voltage regulator for USB power. If you intend to power the board via a 3.3V input, make sure that it is a very clean and regulated supply as anything above 3.6V will damage the ZED-F9P module. The board does have pull-up resistors for the I2C lines so you will not need to worry about logic level translation unless you have other I2C devices on the same bus that operate at different logic levels (eg. 5V).

I cannot say for certain whether or not it will work with the M5 Stack since we do not carry that product but with the right connections, it should work with no issue. Just make sure to run everything at 3.3V.

---

<div class="post-metadata">

**Author:** ![udangpindang](https://avatars.discourse-cdn.com/v4/letter/u/dbc845/32.png) [@udangpindang](https://community.sparkfun.com/u/udangpindang)\
**Post date:** [October 13, 2019, 9:39am UTC](https://community.sparkfun.com/t/qwiic-gps-rtk2-connect-to-grove-port-on-m5stack/37896/3 "2019-10-13T09:39:40Z")

</div>

Thank You Mark, that is clear for now.

I will update the post when it worked.

---

<div class="post-metadata">

**Author:** ![ramsie](https://avatars.discourse-cdn.com/v4/letter/r/f9ae1b/32.png) [@ramsie](https://community.sparkfun.com/u/ramsie)\
**Post date:** [December 4, 2020, 1:43pm UTC](https://community.sparkfun.com/t/qwiic-gps-rtk2-connect-to-grove-port-on-m5stack/37896/4 "2020-12-04T13:43:24Z")

</div>

Hello,

I have an Arduino Uno R3. Its operating voltage is 5V. I want to connect the Arduino to the GPS-RTK2 board via I2C. The operating voltage of the GPS-RTK2 board is 3.3V. I assume that there is 5V at the SDA and SCL connectors.

I supply the GPS-RTK2 board with 3.3V from the Arduino.

Do I need to adjust the SDA connector of the Arduino with a bidirectional level converter to 3.3V to connect it to the SDA connector of the GPS-RTK2 board?

Do I need to set the SCL connector of the Arduino to 3.3V with a bidirectional level converter to connect it to the SCL connector of the GPS-RTK2 board?

Thank you