Qwiic Soil Moisture Sensor SEN-30480 – MX1.25-4P to Qwiic cable

Hello,

I would like to connect a SparkFun Qwiic Soil Moisture Sensor – Capacitive (SEN-30480) to an Elecrow 3.5" 320×480 ESP32 LCD Touch Display.

The Elecrow display has a 4-pin MX1.25 I²C connector providing:

  • 3.3V
  • GND
  • SDA
  • SCL

The SparkFun soil moisture sensor uses the standard Qwiic JST-SH 1.0 mm 4-pin connector.

I am looking for a ready-made cable:

MX1.25-4P → Qwiic / JST-SH 1.0 mm 4P

I would like to connect the sensor directly without soldering, Dupont wires or additional adapters.

Does anyone know a compatible ready-made cable?

If not, could you please confirm the exact required pin/wire order between the two connectors?

I especially need to know whether an available MX1.25-4P → JST-SH 1.0 mm 4P cable can be used straight-through or whether the wires need to be crossed/reordered.

The required electrical connections are:

Elecrow → SparkFun

  • 3.3V → 3.3V
  • GND → GND
  • SDA → SDA
  • SCL → SCL

Elecrow is currently checking the exact physical pin order of their MX1.25-4P connector for me.

Any recommendation for a specific cable or supplier would be greatly appreciated.

Thank you!

Best regards
Daniel

I haven’t seen an adapter with those specs (we do have some that are 2mm pitch to qwiic) :-/

For ours it goes:

Black = GND Red = 3.3V Blue = SDA Yellow = SCL