Hello,
We are designing a power system for a university robot using two QwiicBus EndPoint boards (COM-16988), connected by a 2-metre Cat6 cable, with an MLX90640 sensor at the remote end.
Both boards will use the default 3.3V configuration. What typical and maximum current should we budget for each complete EndPoint board, excluding the sensor, during idle and active I²C communication?
We need the complete board consumption, including termination resistors and the power LED, rather than the PCA9615 IC consumption alone.
Thank you.