So far as I know the maxium consistent power you can have on the 2.4gig band is 100mW eirp. It’s more like 1W in a lot of places, including here, but there ya go, try get all the countries in the world to agree on anything
Ah, hmmm… you’re not moving much data, and this IS the Zigbee protocol. If they have a power averaging testing method, you might be able to boost signal output significantly for that 1-2% duty cycle that Zigbee’s designed for.
I’ve used some FGR-900Mhz radios from Freewave technologies before with good success. Worked just fine at just over a mile with a small whip on one end, and a car mounted reciever on the other. (we didn’t try to go any farther, and I believe that was transmitting at 115Kbaud)
Have you had a chance to try the XBeePro yet? I’m considering it myself for a similar range to yours. Any idea how long the range will be on 10mW (legal maximum in Europe)? Also, my aerial has to be omnidirectional, so I’m stuck with 10mW ERP as well.
For 802.15.4/ZigBee modules, Jennic and Maxstream and a couple of others make 60mW modules. Connected to a 14dBi gain antenna, for both ends of the link, you might get 1-2 miles LINE OF SIGHT. You can do a link budget using one of the on-line calculators. '15.4 will have a longer path length than WiFi because it’s a 2MHz bandwidth (250Kbps) system whereas WiFi 802.11 is 20MHz.
The US FCC limits for EIRP (effective isotropic [antenna radiator] radiated power] is 4 watts, but only with a certain narrow beamwidth. The rules permit increasing power as the antenna directionality increases (reduced potential for interference).
There are (expensive) bi-directional amplifiers for 2.4GHz but they tend to (a) distort the 802.11g OFDM waveform (would not do so for the OQPSK waveform in 802.15.4), and (b) add a lot of noise on the receiver side.