# Reference diameter COM-14966

**URL:** <https://community.sparkfun.com/t/reference-diameter-com-14966/64749>\
**Category:** Other\
**Created:** [April 23, 2025, 7:23am UTC](https://community.sparkfun.com/t/reference-diameter-com-14966/64749 "2025-04-23T07:23:28Z")\
**Posts on this page:** 2\
**Page:** 1

<div class="post-metadata">

**Author:** ![Biolab](https://avatars.discourse-cdn.com/v4/letter/b/50afbb/32.png) [@Biolab](https://community.sparkfun.com/u/Biolab)\
**Post date:** [April 23, 2025, 7:23am UTC](https://community.sparkfun.com/t/reference-diameter-com-14966/64749/1 "2025-04-23T07:23:28Z")

</div>

Hello,

I’m looking for a LED PCB ring that meets the following specifications :

- External diameter of 60.0 mm maximum
- Internal diameter of 45.0 mm minimum
- Essential lighting colors: Red - Green - Blue
- If possible, the device can withstand splashes

I think the COM-14966 model can meet my needs, but I need the following details:

- The inner and outer circular parts of the ring seem to be removable. Is this the case ?
- The inside diameter of the device is not given. Is it possible to have it ?

Thank you in advance for your feedback.

> **[SparkFun LuMini LED Ring - 2 Inch (40 x APA102-2020)](https://www.sparkfun.com/sparkfun-lumini-led-ring-2-inch-40-x-apa102-2020.html)**
>
> The two inch version of the SparkFun LuMini LED Ring, packed with 40 individually addressable LEDS, each capable of producing 16 million colors.

---

<div class="post-metadata">

**Author:** ![TS-Russell](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/ts-russell/32/6092_2.png) [@TS-Russell](https://community.sparkfun.com/u/TS-Russell)\
**Post date:** [April 23, 2025, 7:28am UTC](https://community.sparkfun.com/t/reference-diameter-com-14966/64749/2 "2025-04-23T07:28:43Z")

</div>

According to the [Eagle files](https://cdn.sparkfun.com/assets/c/b/7/b/6/LuMini_2Inch.zip), they are 1.75" (44.45mm) inner diameter, +/- manufacturing tolerances, and 2.13" (54.1mm) outer

So…it’s very close, I’d guess if bought a few some might be 45mm inner. Also note the mounting tabs (canbe removed via saw!) are larger still