# RTK Reference station - bumpy but up and running correctly?

**URL:** <https://community.sparkfun.com/t/rtk-reference-station-bumpy-but-up-and-running-correctly/62787>\
**Category:** SparkPNT / Consumer Products\
**Created:** [January 15, 2025, 7:05pm UTC](https://community.sparkfun.com/t/rtk-reference-station-bumpy-but-up-and-running-correctly/62787 "2025-01-15T19:05:46Z")\
**Posts on this page:** 5\
**Page:** 1

<div class="post-metadata">

**Author:** ![wstefanc](https://avatars.discourse-cdn.com/v4/letter/w/aeb1de/32.png) [@wstefanc](https://community.sparkfun.com/u/wstefanc)\
**Post date:** [January 15, 2025, 7:05pm UTC](https://community.sparkfun.com/t/rtk-reference-station-bumpy-but-up-and-running-correctly/62787/1 "2025-01-15T19:05:46Z")

</div>

It took a bit to get my RTK Reference Station up and running. Setup v4.1 of the firmware, but it didn’t like to change configuration over the WiFi interface. Serial and Ethernet worked fine. Sometimes when it boots now, it fails to start in base mode and displays the last 4 digits of the MAC as 0000 when this happens. The unit then goes into “Rover” mode, if I switch it back from Rover mode to Base, it then starts Base mode fine. Are other folks seeing this? I don’t have the console output handy for when this happens. Will try to capture it in the future, but the unit is outdoors in a somewhat remote location.

Below is what RTK2GO is reporting about my mount point. Is it normal for QZSS to be indicated as “no.” Does the rest of the summary look correct? I have already used corrections from the mount point and they “seem” to be fine. Just looking to double check my configuration.

Also, I have attached a picture of my setup. Mounted the antenna to a a 2" galvanized pipe cap with some threaded rod, nuts, etc. Neatly allowed me to add this to an existing mast.

Any advice / comments appreciated!

Gregg

#### _Messages_

| Msg Format | **RTCM 3.2** |
| --- | --- |
| Messages | **1005(1), 1074(1), 1084(1), 1094(1), 1124(1), 1230(10)** |
| Count | **50,918** total msgs **~5.1** (msg/sec) |
| Signals | GPS: **Yes** GLO: **Yes** QZSS: **No** GAL: **Yes** BeiD: **Yes** WAAS: **No** |
| SV Counts | GPS: **9** GLO: **9** QZSS: **0** GAL: **6** BeiD: **6** WASS: **4** |
| Common GNSS Osc. | **Yes** |

#### Current Caster Table Entry

STR;CastlePeak;Virginia City;RTCM 3.2;1005(1),1074(1),1084(1),1094(1),1124(1),1230(10);0;GPS+GLO+GAL+BDS;SNIP;USA;39.40;-119.65;1;0;sNTRIP;none;B;N;0;none;

 ![41457AD5-AA91-4BD8-882F-C838BA926D51_1_105_c](https://canada1.discourse-cdn.com/sparkfun/original/2X/3/3a60be9f97bc420cd688cdd2f2ba13141e0480ba.jpeg)

---

<div class="post-metadata">

**Author:** ![sparky](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/sparky/32/6021_2.png) [@sparky](https://community.sparkfun.com/u/sparky)\
**Post date:** [January 15, 2025, 10:10pm UTC](https://community.sparkfun.com/t/rtk-reference-station-bumpy-but-up-and-running-correctly/62787/2 "2025-01-15T22:10:24Z")

</div>

Welcome wstefanc!

> Sometimes when it boots now, it fails to start in base mode and displays the last 4 digits of the MAC as 0000 when this happens.

This is most certainly not normal behavior. If you can capture any of the output logs, that would be helpful. I understand the pain of gathering that info from a remote location - I am sorry! If there’s anything specific about your setup you can provide, we can try to replicate the issue.

> Is it normal for QZSS to be indicated as “no.”

Yes. Unless you are in Japan, you will not receive signal from the [QZSS constellation](https://en.wikipedia.org/wiki/Quasi-Zenith_Satellite_System).

---

<div class="post-metadata">

**Author:** ![wstefanc](https://avatars.discourse-cdn.com/v4/letter/w/aeb1de/32.png) [@wstefanc](https://community.sparkfun.com/u/wstefanc)\
**Post date:** [January 15, 2025, 10:41pm UTC](https://community.sparkfun.com/t/rtk-reference-station-bumpy-but-up-and-running-correctly/62787/3 "2025-01-15T22:41:46Z")

</div>

Thanks for the reply and validation of my configuration.

> This is most certainly not normal behavior. If you can capture any of the output logs, that would be helpful. I understand the pain of gathering that info from a remote location - I am sorry! If there’s anything specific about your setup you can provide, we can try to replicate the issue.

Will get out there with a laptop and USB cable in the next day or two to collect the debugging output. Will add that log data to this thread when I have it. There is nothing unique about the installation. I saw the boot issue both on the bench and out in the field so it isn’t an issue with the power out there.

---

<div class="post-metadata">

**Author:** ![PaulZC](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/paulzc/32/67_2.png) [@PaulZC](https://community.sparkfun.com/u/PaulZC)\
**Post date:** [January 16, 2025, 7:35am UTC](https://community.sparkfun.com/t/rtk-reference-station-bumpy-but-up-and-running-correctly/62787/4 "2025-01-16T07:35:03Z")

</div>

Hi Gregg (@wstefanc ),

I just wanted to make you aware that a couple of users have run into RAM issues on the Reference Station recently. I’m not sure if the 0000 issue is RAM related, but it’s a possibility. Links attached below.

I hope this helps,  
Paul

> [@Sparkfun Reference station wifi set up](https://community.sparkfun.com/t/sparkfun-reference-station-wifi-set-up/62625):
>
> I have configured my SparkFun RTK Reference Station to firmware version 4 and set up the SSID and password via serial. The reference station is connected to my network, and the IP address is displayed. However, when I try to connect to the IP address using Putty on my PC, the connection is being rejected. Could you please let me know if any additional configuration is needed to view the NMEA or RTCM messages in my Putty terminal via Wifi?

> [@RTK Reference Station Reboots](https://community.sparkfun.com/t/rtk-reference-station-reboots/62780):
>
> Hello everyone, I am currently commissioning our second RTK Reference Station but have encountered a troubling issue: whenever I enter Survey mode, the station reboots continuously and never completes the process. Originally, the station shipped with firmware 3.5, and I tried upgrading it via the Wi-Fi config page, but it would reboot as soon as I clicked “Install.” As a workaround, I updated the u-blox ZED-F9P module firmware to L1/L2 HPG 1.51 using u-center over USB and then upgraded the Reference Station firmware to 4.1 with RTKUploader over USB. Following these upgrades, the firmware versions displayed correctly on the Ethernet config’s web interface, but after leaving the station off overnight, the Ethernet config page no longer shows the u-blox firmware. Additionally, the Wi-Fi config page still fails to work. Now, whenever I try to cast to RTK2go and switch to Survey mode, the station reboots continuously, never staying on long enough to complete the survey or establish a data…

---

<div class="post-metadata">

**Author:** ![wstefanc](https://avatars.discourse-cdn.com/v4/letter/w/aeb1de/32.png) [@wstefanc](https://community.sparkfun.com/u/wstefanc)\
**Post date:** [January 16, 2025, 4:00pm UTC](https://community.sparkfun.com/t/rtk-reference-station-bumpy-but-up-and-running-correctly/62787/5 "2025-01-16T16:00:12Z")

</div>

Thanks for pointing those out Paul. I had some earlier issues that brought my attention to those posts and memory issues. I have turned of Bluetooth to minimize memory usage. Nothing else seemed to apply. However, I took all the tips to reduce memory usage into consideration from those threads. Hard to believe it has a memory issue when we cold boot but you never know…

Gregg