# Serial baud rate in Qwiic Pro Micro using sample code

**URL:** <https://community.sparkfun.com/t/serial-baud-rate-in-qwiic-pro-micro-using-sample-code/43293>\
**Category:** Arduino\
**Created:** [January 10, 2022, 3:14pm UTC](https://community.sparkfun.com/t/serial-baud-rate-in-qwiic-pro-micro-using-sample-code/43293 "2022-01-10T15:14:33Z")\
**Posts on this page:** 4\
**Page:** 1

<div class="post-metadata">

**Author:** ![sfcaveman](https://avatars.discourse-cdn.com/v4/letter/s/e95f7d/32.png) [@sfcaveman](https://community.sparkfun.com/u/sfcaveman)\
**Post date:** [January 10, 2022, 3:14pm UTC](https://community.sparkfun.com/t/serial-baud-rate-in-qwiic-pro-micro-using-sample-code/43293/1 "2022-01-10T15:14:33Z")

</div>

Using the sample code from [https://learn.sparkfun.com/tutorials/qw … ng-further](https://learn.sparkfun.com/tutorials/qwiic-pro-micro-usb-c-atmega32u4-hookup-guide#resources-and-going-further), the sample code for blinking the TX/RX leds did not send correct serial data out the external serial port (Tx/Rx lines). It looks like the data coming out is the wrong baud rate, although I have tried many different combinations of baud rates, and I am unable to find one where the outputted text is correct. The serial monitor works as expected.

My board is definitely a 5V variant (I saw this on another forum, where they found the devices were 3.3V instead of 5V.

```auto
/* Pro Micro Test Code
   by: Nathan Seidle
   modified by: Jim Lindblom
   SparkFun Electronics
   date: September 16, 2013
   license: Public Domain - please use this code however you'd like.
   It's provided as a learning tool.

   This code is provided to show how to control the SparkFun
   ProMicro's TX and RX LEDs within a sketch. It also serves
   to explain the difference between Serial.print() and
   Serial1.print().
*/

int RXLED = 17; // The RX LED has a defined Arduino pin
// Note: The TX LED was not so lucky, we'll need to use pre-defined
// macros (TXLED1, TXLED0) to control that.
// (We could use the same macros for the RX LED too -- RXLED1,
// and RXLED0.)

void setup()
{
  pinMode(RXLED, OUTPUT); // Set RX LED as an output
  // TX LED is set as an output behind the scenes

  Serial.begin(9600); //This pipes to the serial monitor
  delay(100); // wait for a second
  Serial.println("Initialize Serial Monitor");

  Serial1.begin(9600); //This is the UART, pipes to sensors attached to board
  delay(100); // wait for a second
  Serial1.println("Initialize Serial Hardware UART Pins");
}

void loop()
{
  Serial.println("Hello world!"); // Print "Hello World" to the Serial Monitor
  Serial1.println("Hello! Can anybody hear me?"); // Print "Hello!" over hardware UART

  digitalWrite(RXLED, LOW); // set the RX LED ON
  TXLED0; //TX LED is not tied to a normally controlled pin so a macro is needed, turn LED OFF
  delay(1000); // wait for a second

  digitalWrite(RXLED, HIGH); // set the RX LED OFF
  TXLED1; //TX LED macro to turn LED ON
  delay(1000); // wait for a second
}

```

I do have another serial-related post here, but this issue is completely different than the other. I am trying to get back to the basics to understand the issue.

Also, I noticed that unless I put a delay here:

```auto
  Serial.begin(9600); //This pipes to the serial monitor
  delay(100); // wait for a second
  Serial.println("Initialize Serial Monitor");

```

That the data never gets sent to the monitor. Does this have something to do with the time it takes the USB virtual port setup to complete in Windows after the software is uploaded to the board?

TIA

---

<div class="post-metadata">

**Author:** ![TS-Russell](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/ts-russell/32/6092_2.png) [@TS-Russell](https://community.sparkfun.com/u/TS-Russell)\
**Post date:** [January 12, 2022, 10:15pm UTC](https://community.sparkfun.com/t/serial-baud-rate-in-qwiic-pro-micro-using-sample-code/43293/2 "2022-01-12T22:15:22Z")

</div>

Make sure you have the drivers installed [https://learn.sparkfun.com/tutorials/qw … rs-windows](https://learn.sparkfun.com/tutorials/qwiic-pro-micro-usb-c-atmega32u4-hookup-guide#installing-drivers-windows) and the arduino add-on [https://learn.sparkfun.com/tutorials/qw … up-arduino](https://learn.sparkfun.com/tutorials/qwiic-pro-micro-usb-c-atmega32u4-hookup-guide#setting-up-arduino) and see if that helps

As for the delay, that’s pretty close…here’s an article we have about serial comms/sync [https://learn.sparkfun.com/tutorials/se … 1615791300](https://learn.sparkfun.com/tutorials/serial-communication?_ga=2.175676576.349259513.1641837921-1853259630.1615791300)

---

<div class="post-metadata">

**Author:** ![sfcaveman](https://avatars.discourse-cdn.com/v4/letter/s/e95f7d/32.png) [@sfcaveman](https://community.sparkfun.com/u/sfcaveman)\
**Post date:** [January 14, 2022, 11:46pm UTC](https://community.sparkfun.com/t/serial-baud-rate-in-qwiic-pro-micro-using-sample-code/43293/3 "2022-01-14T23:46:15Z")

</div>

Yes, I did install the drivers and add all of the add-in stuff in. I also double-checked the board is the 5V variant, and I have the 5v variant selected in the drop-down. Thanks for the reply.

---

<div class="post-metadata">

**Author:** ![sfcaveman](https://avatars.discourse-cdn.com/v4/letter/s/e95f7d/32.png) [@sfcaveman](https://community.sparkfun.com/u/sfcaveman)\
**Post date:** [May 19, 2022, 3:54pm UTC](https://community.sparkfun.com/t/serial-baud-rate-in-qwiic-pro-micro-using-sample-code/43293/4 "2022-05-19T15:54:39Z")

</div>

For anyone following this, the fix was to turn on HW handshaking, and then everything works.