# Size incorrect after uploading boards

**URL:** <https://community.sparkfun.com/t/size-incorrect-after-uploading-boards/24944>\
**Category:** BatchPCB\
**Created:** [September 7, 2012, 7:32pm UTC](https://community.sparkfun.com/t/size-incorrect-after-uploading-boards/24944 "2012-09-07T19:32:03Z")\
**Posts on this page:** 6\
**Page:** 1

<div class="post-metadata">

**Author:** ![dan.scof](https://avatars.discourse-cdn.com/v4/letter/d/ad7895/32.png) [@dan.scof](https://community.sparkfun.com/u/dan.scof)\
**Post date:** [September 7, 2012, 7:32pm UTC](https://community.sparkfun.com/t/size-incorrect-after-uploading-boards/24944/1 "2012-09-07T19:32:03Z")

</div>

Hello,

I’ve been working on a board that is 32mm x 32mm. When I upload the board, the images look correct, but somehow the scale seems to be changing. The summary of the board online shows the dimensions as 0.36 x 0.36 (about 1/4 of the actual size).

This seems to be pretty easily reproducible for me. If I start with a new empty board, then:

1. Add a silkscreen box enclosing a 32mm square

2. Add a drill with diameter 4.8mm at position 4mm, 4mm

3. Upload that test file

I see the same issue. The images look correct, but the size shrinks. The site is using the small sizes for the billing cost, too, incidentally.

Has anyone seen something similar or have suggestions on what might be causing it?

---

<div class="post-metadata">

**Author:** ![jmbw](https://avatars.discourse-cdn.com/v4/letter/j/2acd7d/32.png) [@jmbw](https://community.sparkfun.com/u/jmbw)\
**Post date:** [September 7, 2012, 11:08pm UTC](https://community.sparkfun.com/t/size-incorrect-after-uploading-boards/24944/2 "2012-09-07T23:08:27Z")

</div>

I’m having similar trouble. I thought it was because I’ve been using 0-width lines in my .OLN file all this time (because otherwise it bills you for that extra half-line-width sliver all the way around the outside of your board), and the bot’s ability to understand that got broken in the upgrade. But even with a 10-mil outline, the bot appears to totally ignore the .OLN file and computes its own dimensions based on the max/min X/Y of any feature on the board.

Yes the prices come out lower but obviously I’m not going to place an order for a board that might come back with all the edges chopped off (and one previously OK design failed DRC when I re-uploaded, possibly as a result of this truncation, but I can’t be sure since the DRC thingy suddenly doesn’t send email).

Clearly some stuff needs fixing! I assume they’re hard at work on it this very second. Right?

John Wilson

D Bit

---

<div class="post-metadata">

**Author:** ![dan.scof](https://avatars.discourse-cdn.com/v4/letter/d/ad7895/32.png) [@dan.scof](https://community.sparkfun.com/u/dan.scof)\
**Post date:** [September 8, 2012, 12:17am UTC](https://community.sparkfun.com/t/size-incorrect-after-uploading-boards/24944/3 "2012-09-08T00:17:22Z")

</div>

> jmbw:  
> … the bot appears to totally ignore the .OLN file and computes its own dimensions based on the max/min X/Y of any feature on the board.

Looks like you're on to something. If I add a drill hit in the upper right corner, the dimensions get much closer to correct (although still wrong).

Oddly - switching to outline to be a copper trace doesn’t seem to help. Oh well, though. I suppose we just get to wait a few days for things to get fixed.

---

<div class="post-metadata">

**Author:** ![fooj](https://avatars.discourse-cdn.com/v4/letter/f/d07c76/32.png) [@fooj](https://community.sparkfun.com/u/fooj)\
**Post date:** [September 10, 2012, 4:12pm UTC](https://community.sparkfun.com/t/size-incorrect-after-uploading-boards/24944/4 "2012-09-10T16:12:33Z")

</div>

I am having similar issues with my board.

---

<div class="post-metadata">

**Author:** ![checksix](https://avatars.discourse-cdn.com/v4/letter/c/4bbf92/32.png) [@checksix](https://community.sparkfun.com/u/checksix)\
**Post date:** [September 11, 2012, 7:43pm UTC](https://community.sparkfun.com/t/size-incorrect-after-uploading-boards/24944/5 "2012-09-11T19:43:46Z")

</div>

Same problem. An email to support confirmed that it’s a known problem.

---

<div class="post-metadata">

**Author:** ![mrdudeman](https://avatars.discourse-cdn.com/v4/letter/m/46a35a/32.png) [@mrdudeman](https://community.sparkfun.com/u/mrdudeman)\
**Post date:** [November 3, 2012, 7:04pm UTC](https://community.sparkfun.com/t/size-incorrect-after-uploading-boards/24944/6 "2012-11-03T19:04:30Z")

</div>

Did this ever get fixed? I’m still seeing this problem. My boards are not showing up with the correct sizes at all, which makes me hesitant to order anything.