# Sparkfun Thing Plus ESP32-S3 Fails After Good Compile and Download

**URL:** <https://community.sparkfun.com/t/sparkfun-thing-plus-esp32-s3-fails-after-good-compile-and-download/60523>\
**Category:** ESP32\
**Created:** [September 15, 2024, 12:24am UTC](https://community.sparkfun.com/t/sparkfun-thing-plus-esp32-s3-fails-after-good-compile-and-download/60523 "2024-09-15T00:24:32Z")\
**Posts on this page:** 12\
**Page:** 1

<div class="post-metadata">

**Author:** ![KQRR4449](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/kqrr4449/32/6621_2.png) [@KQRR4449](https://community.sparkfun.com/u/KQRR4449)\
**Post date:** [September 15, 2024, 12:24am UTC](https://community.sparkfun.com/t/sparkfun-thing-plus-esp32-s3-fails-after-good-compile-and-download/60523/1 "2024-09-15T00:24:32Z")

</div>

I just received my Thing Plus ESP32-S3. When first powered, the RGB LED faded between colors.  
I set the board and settings following the instructions on the “Arduino Examples” page. I doubled check the board types and made sure the changed settings matched. I left all other setting as is.  
I tried the “RGB Example” and it compiled and downloaded without error.  
The board did not work properly after the download. The RGB LED was a steady green.  
I opened the Serial Monitor and got a rapidly repeating error message. It appears the this line in the error message shows the problem:

E (137) rmt(legacy): CONFLICT! driver\_ng is not allowed to be used with the legacy driver

Can you help me fix this problem?

Thanks very much for your help.

## The full serial output is below:

Rebooting…  
ESP-ROM:esp32s3-20210327  
Build:Mar 27 2021  
rst:0xc (RTC\_SW\_CPU\_RST),boot:0x18 (SPI\_FAST\_FLASH\_BOOT)  
Saved PC:0x40378071  
SPIWP:0xee  
mode:DIO, clock div:1  
load:0x3fce3818,len:0x109c  
load:0x403c9700,len:0x4  
load:0x403c9704,len:0xb50  
load:0x403cc700,len:0x2fd0  
entry 0x403c98ac  
E (137) rmt(legacy): CONFLICT! driver\_ng is not allowed to be used with the legacy driver

abort() was called at PC 0x4200920b on core 0

Backtrace: 0x40377a5e:0x3fceb200 0x4037c8dd:0x3fceb220 0x40382471:0x3fceb240 0x4200920b:0x3fceb2c0 0x4200cee6:0x3fceb2e0 0x40377d63:0x3fceb310 0x403cdb0a:0x3fceb340 0x403cdea1:0x3fceb380 0x403c9919:0x3fceb4b0 0x40045c01:0x3fceb570 0x40043ab6:0x3fceb6f0 0x40034c45:0x3fceb710

ELF file SHA256: 126c11852c22b594

E (166) esp\_core\_dump\_flash: Core dump flash config is corrupted! CRC=0x7bd5c66f instead of 0x0  
E (174) esp\_core\_dump\_elf: Elf write init failed!  
E (179) esp\_core\_dump\_common: Core dump write failed with error=-1

---

<div class="post-metadata">

**Author:** ![TS-Russell](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/ts-russell/32/6092_2.png) [@TS-Russell](https://community.sparkfun.com/u/TS-Russell)\
**Post date:** [September 16, 2024, 11:49pm UTC](https://community.sparkfun.com/t/sparkfun-thing-plus-esp32-s3-fails-after-good-compile-and-download/60523/2 "2024-09-16T23:49:44Z")

</div>

The error you’re encountering is related to a conflict between different versions of the RMT (Remote Control) driver in the ESP32-S3. The message “CONFLICT! driver\_ng is not allowed to be used with the legacy driver” suggests that there’s a mismatch between the driver versions being used.

To resolve this issue, you can try the following steps:

1. Update your ESP32 Arduino core:  
Make sure you have the latest version of the ESP32 Arduino core installed. You can do this by:

2. Check your code for RMT usage:  
If you’re using any RMT-related functions in your code, make sure you’re consistently using either the legacy or the new generation (ng) version, not both.

3. Modify the Arduino JSON files:  
If the problem persists, you might need to modify some configuration files:

4. Use a different LED library:  
If you’re using a specific LED library that might be causing this conflict, try using a different one or implement the LED control manually.

5. Check board settings:  
Ensure that you have selected the correct board in the Arduino IDE:

- USB Mode: Hardware CDC and JTAG
- USB CDC on Boot: Enabled
- Upload Mode: UART0 / Hardware CDC
- PSRAM: QSPI PSRAM  
are all set

1. Try a simple blink sketch:  
If the problem persists, try uploading a simple blink sketch without using the RGB LED to see if the board is functioning correctly otherwise

---

<div class="post-metadata">

**Author:** ![KQRR4449](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/kqrr4449/32/6621_2.png) [@KQRR4449](https://community.sparkfun.com/u/KQRR4449)\
**Post date:** [September 18, 2024, 12:47am UTC](https://community.sparkfun.com/t/sparkfun-thing-plus-esp32-s3-fails-after-good-compile-and-download/60523/3 "2024-09-18T00:47:14Z")

</div>

This was not a program I wrote but the “RGB LED Example” sketch provided on the Sparkfun Thing Plus ESP32-S3 examples page at:  
[https://docs.sparkfun.com/SparkFun\_Thing\_Plus\_ESP32-S3/arduino\_example/#thing-plus-esp32-s3-github-repository](https://docs.sparkfun.com/SparkFun_Thing_Plus_ESP32-S3/arduino_example/#thing-plus-esp32-s3-github-repository)

This sketch was written by:

```auto
  By: Nathan Seidle
  SparkFun Electronics
  Date: January 13, 2024

```

I verified that my ESP32 board was the latest revision 3.0.4. I also made sure all the libraries were up to date including the FastLED library at revision 3.7.7.

I could not find the json file you mentioned at the path:  
“C:\Users[YOUR\_USER\_NAME]\AppData\Local\Arduino15”  
so I was unable to modify:  
“#define SOC\_RMT\_CHANNELS\_PER\_GROUP (1)”

I did verify that the blink sketchran correctly but the LED did not blink since only the RGB LED was present. I added some print statements and verified the code was executing properly.

Could you check with Nathan and see if he has any suggestions to get his sketch to work.

---

<div class="post-metadata">

**Author:** ![KQRR4449](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/kqrr4449/32/6621_2.png) [@KQRR4449](https://community.sparkfun.com/u/KQRR4449)\
**Post date:** [September 18, 2024, 11:43pm UTC](https://community.sparkfun.com/t/sparkfun-thing-plus-esp32-s3-fails-after-good-compile-and-download/60523/4 "2024-09-18T23:43:54Z")

</div>

I have some additional information.  
The problem appears to be in the FastLED library. I get the same error with several of the example sketches supplied with this library.  
I tried using the “Adafruit NeoPixel” version 1.12.3 library based on a Google suggestion and this library appears to work.  
There appears to be several libraries that are variants of the FastLED library. I am using version 3.7.7 which is the latest Arduino update.  
**Could you tell me which version of the FastLED library Nathan used?**

---

<div class="post-metadata">

**Author:** ![TS-Russell](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/ts-russell/32/6092_2.png) [@TS-Russell](https://community.sparkfun.com/u/TS-Russell)\
**Post date:** [September 19, 2024, 5:11pm UTC](https://community.sparkfun.com/t/sparkfun-thing-plus-esp32-s3-fails-after-good-compile-and-download/60523/5 "2024-09-19T17:11:33Z")

</div>

Going purely by the date (Jan 2024) [my first guess is 3.6](https://github.com/FastLED/FastLED/releases) - try that and see if it improves things…not sure if you’d need the ESP-IDF from that same time period or not [(4.7?)](https://github.com/espressif/esptool/releases/tag/v4.7.0)

Give those a try as a last resort and I’ll try to poke Nathan if that doesn’t work 🙂

---

<div class="post-metadata">

**Author:** ![KQRR4449](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/kqrr4449/32/6621_2.png) [@KQRR4449](https://community.sparkfun.com/u/KQRR4449)\
**Post date:** [September 21, 2024, 11:06pm UTC](https://community.sparkfun.com/t/sparkfun-thing-plus-esp32-s3-fails-after-good-compile-and-download/60523/6 "2024-09-21T23:06:08Z")

</div>

I first tried using FastLED version 3.7.7 with an original ESP32 chip in a DOIT ESP32 DEVKIT V1. The program compiled and loaded into to board without error. All I got was the ESP32 boot messages followed by my starting println(). I did not get any run time errors. I did not have a WS2812B to test that the board was generating the correct output but things looked good.

I next downgraded my FastLED library to version 3.6.0 and tried to compile the sketch. I got a large number of errors having to do with missing variables, etc. I tried FastLED version 3.6.0 with both the ESP32-S3 and the ESP32. Both gave similar error messages except that the ESP32-S3 had two additional blocks of error messages toward the end of error messages.

It is likely that I would need to downgrade a number of libraries and possibly the board definitions to get FastLED version 3.6.0 to compile.

I have attached the ESP32-S3 error messages for FastLED version 3.6.0 below. I can send the ESP32 error message if you would like.

Sincerely,

Ken West

---------------------------- FastLED Version 3.6.0 Compile Errors for ESP32-S3 -----------------------

In file included from C:\Users\kenw\Documents\Arduino\libraries\FastLED\src/FastLED.h:75,  
from C:\Users\kenw\Documents\Arduino\ESP32S3\Sparkfun\Sparkfun Thing Plus - ESP32-S3\RGB\_LED\_ESP32S3\RGB\_LED\_ESP32S3.ino:23:  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src/fastspi.h:157:23: note: ‘#pragma message: No hardware SPI pins defined. All SPI access will default to bitbanged output’  
157 | # pragma message “No hardware SPI pins defined. All SPI access will default to bitbanged output”  
| ^ ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\noise.cpp: In function ‘void fill\_raw\_2dnoise8(uint8\_t\*, int, int, uint8\_t, q44, fract8, int, uint16\_t, int, uint16\_t, int, uint16\_t)’:  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\noise.cpp:623:100: error: ambiguous overload for ‘operator\*’ (operand types are ‘q44’ {aka ‘q\<unsigned char, 4, 4\>’} and ‘int’)  
623 | fill\_raw\_2dnoise8(pData, width, height, octaves-1, freq44, amplitude, skip+1, x_freq44, freq44 \* scalex, y_freq44, freq44 \* scaley, time);  
| ~~~~~~^~~~~~~  
| | |  
| | int  
| q44 {aka q\<unsigned char, 4, 4\>}  
In file included from C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\pixeltypes.h:7,  
from C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\controller.h:9,  
from C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\FastLED.h:57,  
from C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\noise.cpp:6:  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:909:14: note: candidate: ‘uint32\_t q\<T, F, I\>::operator\*(uint32\_t) [with T = unsigned char; int F = 4; int I = 4; uint32\_t = long unsigned int]’  
909 | uint32\_t operator\*(uint32\_t v) { return (v_i) + ((v_f)\>\>F); }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:911:14: note: candidate: ‘uint16\_t q\<T, F, I\>::operator\*(uint16\_t) [with T = unsigned char; int F = 4; int I = 4; uint16\_t = short unsigned int]’  
911 | uint16\_t operator\*(uint16\_t v) { return (v_i) + ((v_f)\>\>F); }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:913:13: note: candidate: ‘int32\_t q\<T, F, I\>::operator\*(int32\_t) [with T = unsigned char; int F = 4; int I = 4; int32\_t = long int]’  
913 | int32\_t operator\*(int32\_t v) { return (v_i) + ((v_f)\>\>F); }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:915:13: note: candidate: ‘int16\_t q\<T, F, I\>::operator\*(int16\_t) [with T = unsigned char; int F = 4; int I = 4; int16\_t = short int]’  
915 | int16\_t operator\*(int16\_t v) { return (v_i) + ((v_f)\>\>F); }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\noise.cpp:623:127: error: ambiguous overload for ‘operator\*’ (operand types are ‘q44’ {aka ‘q\<unsigned char, 4, 4\>’} and ‘int’)  
623 | fill\_raw\_2dnoise8(pData, width, height, octaves-1, freq44, amplitude, skip+1, x_freq44, freq44 \* scalex, y_freq44, freq44 \* scaley, time);  
| ~~~~~~^~~~~~~  
| | |  
| | int  
| q44 {aka q\<unsigned char, 4, 4\>}  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:909:14: note: candidate: ‘uint32\_t q\<T, F, I\>::operator\*(uint32\_t) [with T = unsigned char; int F = 4; int I = 4; uint32\_t = long unsigned int]’  
909 | uint32\_t operator\*(uint32\_t v) { return (v_i) + ((v_f)\>\>F); }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:911:14: note: candidate: ‘uint16\_t q\<T, F, I\>::operator\*(uint16\_t) [with T = unsigned char; int F = 4; int I = 4; uint16\_t = short unsigned int]’  
911 | uint16\_t operator\*(uint16\_t v) { return (v_i) + ((v_f)\>\>F); }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:913:13: note: candidate: ‘int32\_t q\<T, F, I\>::operator\*(int32\_t) [with T = unsigned char; int F = 4; int I = 4; int32\_t = long int]’  
913 | int32\_t operator\*(int32\_t v) { return (v_i) + ((v_f)\>\>F); }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:915:13: note: candidate: ‘int16\_t q\<T, F, I\>::operator\*(int16\_t) [with T = unsigned char; int F = 4; int I = 4; int16\_t = short int]’  
915 | int16\_t operator\*(int16\_t v) { return (v_i) + ((v_f)\>\>F); }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\noise.cpp: In function ‘void fill\_raw\_2dnoise16(uint16\_t\*, int, int, uint8\_t, q88, fract16, int, uint32\_t, int, uint32\_t, int, uint32\_t)’:  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\noise.cpp:661:101: error: ambiguous overload for ‘operator\*’ (operand types are ‘int’ and ‘q88’ {aka ‘q\<short unsigned int, 8, 8\>’})  
661 | fill\_raw\_2dnoise16(pData, width, height, octaves-1, freq88, amplitude, skip, x _freq88 , scalex freq88, y \* freq88, scaley \* freq88, time);  
| ~~~~~~^~~~~~~  
| | |  
| int q88 {aka q\<short unsigned int, 8, 8\>}  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:922:49: note: candidate: 'uint32\_t operator(uint32\_t, q\<T, F, I\>&) [with T = short unsigned int; int F = 8; int I = 8; uint32\_t = long unsigned int]’  
922 | template\<class T, int F, int I\> static uint32\_t operator_(uint32\_t v, q\<T,F,I\> & q) { return q \* v; }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:923:49: note: candidate: ‘uint16\_t operator\*(uint16\_t, q\<T, F, I\>&) [with T = short unsigned int; int F = 8; int I = 8; uint16\_t = short unsigned int]’  
923 | template\<class T, int F, int I\> static uint16\_t operator\*(uint16\_t v, q\<T,F,I\> & q) { return q \* v; }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:924:48: note: candidate: ‘int32\_t operator\*(int32\_t, q\<T, F, I\>&) [with T = short unsigned int; int F = 8; int I = 8; int32\_t = long int]’  
924 | template\<class T, int F, int I\> static int32\_t operator\*(int32\_t v, q\<T,F,I\> & q) { return q \* v; }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:925:48: note: candidate: ‘int16\_t operator\*(int16\_t, q\<T, F, I\>&) [with T = short unsigned int; int F = 8; int I = 8; int16\_t = short int]’  
925 | template\<class T, int F, int I\> static int16\_t operator\*(int16\_t v, q\<T,F,I\> & q) { return q \* v; }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\noise.cpp:661:129: error: ambiguous overload for ‘operator\*’ (operand types are ‘int’ and ‘q88’ {aka ‘q\<short unsigned int, 8, 8\>’})  
661 | fill\_raw\_2dnoise16(pData, width, height, octaves-1, freq88, amplitude, skip, x _freq88 , scalex freq88, y \* freq88, scaley \* freq88, time);  
| ~~~~~~^~~~~~~  
| | |  
| int q88 {aka q\<short unsigned int, 8, 8\>}  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:922:49: note: candidate: 'uint32\_t operator(uint32\_t, q\<T, F, I\>&) [with T = short unsigned int; int F = 8; int I = 8; uint32\_t = long unsigned int]’  
922 | template\<class T, int F, int I\> static uint32\_t operator_(uint32\_t v, q\<T,F,I\> & q) { return q \* v; }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:923:49: note: candidate: ‘uint16\_t operator\*(uint16\_t, q\<T, F, I\>&) [with T = short unsigned int; int F = 8; int I = 8; uint16\_t = short unsigned int]’  
923 | template\<class T, int F, int I\> static uint16\_t operator\*(uint16\_t v, q\<T,F,I\> & q) { return q \* v; }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:924:48: note: candidate: ‘int32\_t operator\*(int32\_t, q\<T, F, I\>&) [with T = short unsigned int; int F = 8; int I = 8; int32\_t = long int]’  
924 | template\<class T, int F, int I\> static int32\_t operator\*(int32\_t v, q\<T,F,I\> & q) { return q \* v; }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:925:48: note: candidate: ‘int16\_t operator\*(int16\_t, q\<T, F, I\>&) [with T = short unsigned int; int F = 8; int I = 8; int16\_t = short int]’  
925 | template\<class T, int F, int I\> static int16\_t operator\*(int16\_t v, q\<T,F,I\> & q) { return q \* v; }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\noise.cpp: In function ‘void fill\_raw\_2dnoise16into8(uint8\_t\*, int, int, uint8\_t, q44, fract8, int, uint32\_t, int, uint32\_t, int, uint32\_t)’:  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\noise.cpp:699:106: error: ambiguous overload for ‘operator\*’ (operand types are ‘int’ and ‘q44’ {aka ‘q\<unsigned char, 4, 4\>’})  
699 | fill\_raw\_2dnoise16into8(pData, width, height, octaves-1, freq44, amplitude, skip+1, x_freq44, scalex freq44, yfreq44, scaley \* freq44, time);  
| ~~~~~~^~~~~~~  
| | |  
| int q44 {aka q\<unsigned char, 4, 4\>}  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:922:49: note: candidate: 'uint32\_t operator_(uint32\_t, q\<T, F, I\>&) [with T = unsigned char; int F = 4; int I = 4; uint32\_t = long unsigned int]’  
922 | template\<class T, int F, int I\> static uint32\_t operator\*(uint32\_t v, q\<T,F,I\> & q) { return q \* v; }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:923:49: note: candidate: ‘uint16\_t operator\*(uint16\_t, q\<T, F, I\>&) [with T = unsigned char; int F = 4; int I = 4; uint16\_t = short unsigned int]’  
923 | template\<class T, int F, int I\> static uint16\_t operator\*(uint16\_t v, q\<T,F,I\> & q) { return q \* v; }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:924:48: note: candidate: ‘int32\_t operator\*(int32\_t, q\<T, F, I\>&) [with T = unsigned char; int F = 4; int I = 4; int32\_t = long int]’  
924 | template\<class T, int F, int I\> static int32\_t operator\*(int32\_t v, q\<T,F,I\> & q) { return q \* v; }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:925:48: note: candidate: ‘int16\_t operator\*(int16\_t, q\<T, F, I\>&) [with T = unsigned char; int F = 4; int I = 4; int16\_t = short int]’  
925 | template\<class T, int F, int I\> static int16\_t operator\*(int16\_t v, q\<T,F,I\> & q) { return q \* v; }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\noise.cpp:699:132: error: ambiguous overload for ‘operator\*’ (operand types are ‘int’ and ‘q44’ {aka ‘q\<unsigned char, 4, 4\>’})  
699 | fill\_raw\_2dnoise16into8(pData, width, height, octaves-1, freq44, amplitude, skip+1, x_freq44, scalex freq44, yfreq44, scaley \* freq44, time);  
| ~~~~~~^~~~~~~  
| | |  
| int q44 {aka q\<unsigned char, 4, 4\>}  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:922:49: note: candidate: 'uint32\_t operator_(uint32\_t, q\<T, F, I\>&) [with T = unsigned char; int F = 4; int I = 4; uint32\_t = long unsigned int]’  
922 | template\<class T, int F, int I\> static uint32\_t operator\*(uint32\_t v, q\<T,F,I\> & q) { return q \* v; }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:923:49: note: candidate: ‘uint16\_t operator\*(uint16\_t, q\<T, F, I\>&) [with T = unsigned char; int F = 4; int I = 4; uint16\_t = short unsigned int]’  
923 | template\<class T, int F, int I\> static uint16\_t operator\*(uint16\_t v, q\<T,F,I\> & q) { return q \* v; }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:924:48: note: candidate: ‘int32\_t operator\*(int32\_t, q\<T, F, I\>&) [with T = unsigned char; int F = 4; int I = 4; int32\_t = long int]’  
924 | template\<class T, int F, int I\> static int32\_t operator\*(int32\_t v, q\<T,F,I\> & q) { return q \* v; }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\lib8tion.h:925:48: note: candidate: ‘int16\_t operator\*(int16\_t, q\<T, F, I\>&) [with T = unsigned char; int F = 4; int I = 4; int16\_t = short int]’  
925 | template\<class T, int F, int I\> static int16\_t operator\*(int16\_t v, q\<T,F,I\> & q) { return q \* v; }  
| ^ ~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\platforms\esp\32\clockless\_rmt\_esp32.cpp: In member function ‘void ESP32RMTController::startOnChannel(int)’:  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\platforms\esp\32\clockless\_rmt\_esp32.cpp:266:29: error: ‘RMTMEM’ was not declared in this scope  
266 | mRMT\_mem\_start = & (RMTMEM.chan[mRMT\_channel].data32[0].val);  
| ^ ~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\platforms\esp\32\clockless\_rmt\_esp32.cpp: In member function ‘void ESP32RMTController::tx\_start()’:  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\platforms\esp\32\clockless\_rmt\_esp32.cpp:307:32: error: ‘volatile union rmt\_chnconf0\_reg\_t’ has no member named ‘mem\_rd\_rst\_n’  
307 | RMT.chnconf0[mRMT\_channel].mem\_rd\_rst\_n = 1;  
| ^ ~~~~~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\platforms\esp\32\clockless\_rmt\_esp32.cpp:308:32: error: ‘volatile union rmt\_chnconf0\_reg\_t’ has no member named ‘mem\_rd\_rst\_n’  
308 | RMT.chnconf0[mRMT\_channel].mem\_rd\_rst\_n = 0;  
| ^ ~~~~~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\platforms\esp\32\clockless\_rmt\_esp32.cpp:309:32: error: ‘volatile union rmt\_chnconf0\_reg\_t’ has no member named ‘apb\_mem\_rst\_n’  
309 | RMT.chnconf0[mRMT\_channel].apb\_mem\_rst\_n = 1;  
| ^ ~~~~~~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\platforms\esp\32\clockless\_rmt\_esp32.cpp:310:32: error: ‘volatile union rmt\_chnconf0\_reg\_t’ has no member named ‘apb\_mem\_rst\_n’  
310 | RMT.chnconf0[mRMT\_channel].apb\_mem\_rst\_n = 0;  
| ^ ~~~~~~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\platforms\esp\32\clockless\_rmt\_esp32.cpp:316:32: error: ‘volatile union rmt\_chnconf0\_reg\_t’ has no member named ‘conf\_update\_n’  
316 | RMT.chnconf0[mRMT\_channel].conf\_update\_n = 1;  
| ^ ~~~~~~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\platforms\esp\32\clockless\_rmt\_esp32.cpp:317:32: error: ‘volatile union rmt\_chnconf0\_reg\_t’ has no member named ‘tx\_start\_n’  
317 | RMT.chnconf0[mRMT\_channel].tx\_start\_n = 1;  
| ^ ~~~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\platforms\esp\32\clockless\_rmt\_esp32.cpp: In static member function ‘static void ESP32RMTController::doneOnChannel(rmt\_channel\_t, void\*)’:  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\platforms\esp\32\clockless\_rmt\_esp32.cpp:347:5: error: ‘gpio\_matrix\_out’ was not declared in this scope; did you mean ‘gpio\_iomux\_out’?  
347 | gpio\_matrix\_out(pController-\>mPin, 0x100, 0, 0);  
| ^ ~~~~~~~~~~~~~~  
| gpio\_iomux\_out  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\platforms\esp\32\clockless\_rmt\_esp32.cpp:368:27: error: ‘volatile union rmt\_chnconf0\_reg\_t’ has no member named ‘tx\_stop\_n’  
368 | RMT.chnconf0[channel].tx\_stop\_n = 1;  
| ^ ~~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\platforms\esp\32\clockless\_rmt\_esp32.cpp:369:27: error: ‘volatile union rmt\_chnconf0\_reg\_t’ has no member named ‘conf\_update\_n’  
369 | RMT.chnconf0[channel].conf\_update\_n = 1;  
| ^ ~~~~~~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\platforms\esp\32\clockless\_rmt\_esp32.cpp:371:27: error: ‘volatile union rmt\_chnconf0\_reg\_t’ has no member named ‘mem\_rd\_rst\_n’  
371 | RMT.chnconf0[channel].mem\_rd\_rst\_n = 1;  
| ^ ~~~~~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\platforms\esp\32\clockless\_rmt\_esp32.cpp:372:27: error: ‘volatile union rmt\_chnconf0\_reg\_t’ has no member named ‘mem\_rd\_rst\_n’  
372 | RMT.chnconf0[channel].mem\_rd\_rst\_n = 0;  
| ^ ~~~~~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\platforms\esp\32\clockless\_rmt\_esp32.cpp:373:27: error: ‘volatile union rmt\_chnconf0\_reg\_t’ has no member named ‘apb\_mem\_rst\_n’  
373 | RMT.chnconf0[channel].apb\_mem\_rst\_n = 1;  
| ^ ~~~~~~~~~~~~  
C:\Users\kenw\Documents\Arduino\libraries\FastLED\src\platforms\esp\32\clockless\_rmt\_esp32.cpp:374:27: error: ‘volatile union rmt\_chnconf0\_reg\_t’ has no member named ‘apb\_mem\_rst\_n’  
374 | RMT.chnconf0[channel].apb\_mem\_rst\_n = 0;  
| ^ ~~~~~~~~~~~~

exit status 1

Compilation error: exit status 1

---

<div class="post-metadata">

**Author:** ![TS-Russell](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/ts-russell/32/6092_2.png) [@TS-Russell](https://community.sparkfun.com/u/TS-Russell)\
**Post date:** [September 24, 2024, 11:18pm UTC](https://community.sparkfun.com/t/sparkfun-thing-plus-esp32-s3-fails-after-good-compile-and-download/60523/7 "2024-09-24T23:18:35Z")

</div>

I suspect you are right…or test on a fresh separate PC/laptop, or create a backup copy of the arduino15 folder and wipe the main one to begin anew…are either of those workable?

---

<div class="post-metadata">

**Author:** ![KQRR4449](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/kqrr4449/32/6621_2.png) [@KQRR4449](https://community.sparkfun.com/u/KQRR4449)\
**Post date:** [September 25, 2024, 12:35am UTC](https://community.sparkfun.com/t/sparkfun-thing-plus-esp32-s3-fails-after-good-compile-and-download/60523/8 "2024-09-25T00:35:10Z")

</div>

I actually installed the Arduino IDE from scratch so things should be good. I have tried several other WS2812 libraries and they worked fine. Is there any chance Nathan Seidle would have time to identify which version of the FastLED he used.

---

<div class="post-metadata">

**Author:** ![TS-Russell](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/ts-russell/32/6092_2.png) [@TS-Russell](https://community.sparkfun.com/u/TS-Russell)\
**Post date:** [September 26, 2024, 8:06pm UTC](https://community.sparkfun.com/t/sparkfun-thing-plus-esp32-s3-fails-after-good-compile-and-download/60523/9 "2024-09-26T20:06:14Z")

</div>

I sent a message - give it a few days and hopefully we’ll know more soon 🙂

---

<div class="post-metadata">

**Author:** ![TS-Russell](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/ts-russell/32/6092_2.png) [@TS-Russell](https://community.sparkfun.com/u/TS-Russell)\
**Post date:** [September 27, 2024, 6:24pm UTC](https://community.sparkfun.com/t/sparkfun-thing-plus-esp32-s3-fails-after-good-compile-and-download/60523/10 "2024-09-27T18:24:05Z")

</div>

So, I’m unsure as to whether I’d consider this good news or not at this point, but:  
 ![image](https://canada1.discourse-cdn.com/sparkfun/original/2X/6/645650ded3f83c8a72655d9f22413e3c192e2fe8.png)

---

<div class="post-metadata">

**Author:** ![KQRR4449](https://yyz1.discourse-cdn.com/sparkfun/user_avatar/community.sparkfun.com/kqrr4449/32/6621_2.png) [@KQRR4449](https://community.sparkfun.com/u/KQRR4449)\
**Post date:** [September 28, 2024, 1:06am UTC](https://community.sparkfun.com/t/sparkfun-thing-plus-esp32-s3-fails-after-good-compile-and-download/60523/11 "2024-09-28T01:06:18Z")

</div>

Sadly, i tried downgrading FastLED to version 3.6.0 but I got a lot of compile errors. I listed these in a previous post. I suspect I would need to downgrade a large number of libraries to use version 3.6.0.

I had been using FastLED version 3.77 for most of the tests. They recently updated it to 3.7.8 and I repeated the tests. The code still compiles but I get the same abort code when the ESP32-S3 tries to run it.

I would suggest removing the FastLED library example from your example code since it fails with later versions of FastLED. You can add it back when it is working.

---

<div class="post-metadata">

**Author:** ![dwkennedy](https://avatars.discourse-cdn.com/v4/letter/d/3ec8ea/32.png) [@dwkennedy](https://community.sparkfun.com/u/dwkennedy)\
**Post date:** [November 7, 2024, 9:12pm UTC](https://community.sparkfun.com/t/sparkfun-thing-plus-esp32-s3-fails-after-good-compile-and-download/60523/12 "2024-11-07T21:12:27Z")

</div>

I’m getting the same results (green when it should be black and other weirdness)  
Adafruit Neopixel library works so I will go with that for now.

Arduino IDE 2.3.3, fastled 3.9.2, adafruit neopixel 1.12.3. i didn’t try older versions of FastLED